sl_bt_evt_connection_parametersConnection
Triggered whenever the connection parameters are changed and at any time a connection is established.
Data Structures | |
struct | sl_bt_evt_connection_parameters_s |
Data structure of the parameters event. | |
Macros | |
#define | sl_bt_evt_connection_parameters_id 0x020600a0 |
Identifier of the parameters event. | |
Detailed Description
Triggered whenever the connection parameters are changed and at any time a connection is established.
Data Structure Documentation
◆ sl_bt_evt_connection_parameters_s
struct sl_bt_evt_connection_parameters_s |
Data structure of the parameters event.
Data Fields | ||
---|---|---|
uint8_t | connection |
Connection handle |
uint16_t | interval |
Connection interval. Time = Value x 1.25 ms |
uint16_t | latency |
Peripheral latency (how many connection intervals the peripheral can skip) |
uint16_t | timeout |
Supervision timeout. Time = Value x 10 ms |
uint8_t | security_mode |
Enum sl_bt_connection_security_t. Connection security mode. Values:
|
uint16_t | txsize |
Maximum Data Channel PDU Payload size that the controller can send in an air packet |