sl_bt_evt_connection_remote_used_featuresConnection
List of link layer features supported by the remote device.
Data Structures | |
struct | sl_bt_evt_connection_remote_used_features_s |
Data structure of the remote_used_features event. | |
Macros | |
#define | sl_bt_evt_connection_remote_used_features_id 0x080600a0 |
Identifier of the remote_used_features event. | |
Detailed Description
List of link layer features supported by the remote device.
Data Structure Documentation
◆ sl_bt_evt_connection_remote_used_features_s
struct sl_bt_evt_connection_remote_used_features_s |
Data structure of the remote_used_features event.
Data Fields | ||
---|---|---|
uint8_t | connection |
Connection handle |
uint8array | features |
This parameter is 8 bytes in little endian format and contains bit fields describing the supported link layer features of the remote device. Bit value 1 means that the feature is supported. The bits are explained in Bluetooth specification Vol 6, Part B, 4.6. |