sl_bt_evt_dfu_boot_failureDevice Firmware Update

This event indicates that an error, which prevents the device from booting, has occurred in bootloader.

Data Structures

struct  sl_bt_evt_dfu_boot_failure_s
 Data structure of the boot_failure event.
 

Macros

#define sl_bt_evt_dfu_boot_failure_id   0x010000a0
 Identifier of the boot_failure event.
 

Detailed Description

This event indicates that an error, which prevents the device from booting, has occurred in bootloader.


Data Structure Documentation

◆ sl_bt_evt_dfu_boot_failure_s

struct sl_bt_evt_dfu_boot_failure_s

Data structure of the boot_failure event.

Data Fields
uint16_t reason

The reason for boot failure.