sl_bt_evt_gatt_descriptorGATT Client
Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.
Data Structures | |
struct | sl_bt_evt_gatt_descriptor_s |
Data structure of the descriptor event. | |
Macros | |
#define | sl_bt_evt_gatt_descriptor_id 0x030900a0 |
Identifier of the descriptor event. | |
Detailed Description
Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.
It is generated after issuing the sl_bt_gatt_discover_descriptors command.
Data Structure Documentation
◆ sl_bt_evt_gatt_descriptor_s
struct sl_bt_evt_gatt_descriptor_s |
Data structure of the descriptor event.
Data Fields | ||
---|---|---|
uint8_t | connection |
Connection handle |
uint16_t | descriptor |
GATT characteristic descriptor handle |
uint8array | uuid |
Descriptor UUID in little endian format |