sl_bt_evt_gatt_descriptor_valueGATT Client

Indicates that the value of a descriptor in the remote GATT server was received.

Data Structures

struct  sl_bt_evt_gatt_descriptor_value_s
 Data structure of the descriptor_value event.
 

Macros

#define sl_bt_evt_gatt_descriptor_value_id   0x050900a0
 Identifier of the descriptor_value event.
 

Detailed Description

Indicates that the value of a descriptor in the remote GATT server was received.

This event is generated by the sl_bt_gatt_read_descriptor_value command.


Data Structure Documentation

◆ sl_bt_evt_gatt_descriptor_value_s

struct sl_bt_evt_gatt_descriptor_value_s

Data structure of the descriptor_value event.

Data Fields
uint8_t connection

Connection handle

uint16_t descriptor

GATT characteristic descriptor handle

uint16_t offset

Value offset

uint8array value

Descriptor value