sl_bt_evt_gatt_server_characteristic_statusGATT Server
Indicates either that a local Client Characteristic Configuration descriptor was changed by the remote GATT client, or that a confirmation from the remote GATT client was received upon a successful reception of the indication.
Data Structures | |
struct | sl_bt_evt_gatt_server_characteristic_status_s |
Data structure of the characteristic_status event. | |
Macros | |
#define | sl_bt_evt_gatt_server_characteristic_status_id 0x030a00a0 |
Identifier of the characteristic_status event. | |
Detailed Description
Indicates either that a local Client Characteristic Configuration descriptor was changed by the remote GATT client, or that a confirmation from the remote GATT client was received upon a successful reception of the indication.
A confirmation by the remote GATT client should be received within 30 seconds after an indication was sent with the sl_bt_gatt_server_send_indication command, otherwise further GATT transactions over this connection are not allowed by the stack.
Data Structure Documentation
◆ sl_bt_evt_gatt_server_characteristic_status_s
struct sl_bt_evt_gatt_server_characteristic_status_s |
Data structure of the characteristic_status event.
Data Fields | ||
---|---|---|
uint8_t | connection |
Connection handle |
uint16_t | characteristic |
GATT characteristic handle. This value is normally received from the gatt_characteristic event. |
uint8_t | status_flags |
Enum sl_bt_gatt_server_characteristic_status_flag_t. Describes whether Client Characteristic Configuration was changed or if a confirmation was received. Values:
|
uint16_t | client_config_flags |
Enum sl_bt_gatt_server_client_configuration_t. This field carries the new value of the Client Characteristic Configuration. If the status_flags is 0x2 (confirmation received), the value of this field can be ignored. |
uint16_t | client_config |
The handle of client-config descriptor. |