sl_bt_evt_sync_closedSynchronization

Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.

Data Structures

struct  sl_bt_evt_sync_closed_s
 Data structure of the closed event.
 

Macros

#define sl_bt_evt_sync_closed_id   0x014200a0
 Identifier of the closed event.
 

Detailed Description

Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.

The synchronization establishment procedure can be canceled explicitly by the application by issuing command sl_bt_sync_close, or internally due to synchronization failing. Synchronization can fail for example due to incompatible sync CTE type.


Data Structure Documentation

◆ sl_bt_evt_sync_closed_s

struct sl_bt_evt_sync_closed_s

Data structure of the closed event.

Data Fields
uint16_t reason

Result code

  • 0: success
  • Non-zero: an error has occurred
uint16_t sync

Periodic advertising synchronization handle