sl_bt_evt_system_bootSystem

Indicates that the device has started and the radio is ready.

Data Structures

struct  sl_bt_evt_system_boot_s
 Data structure of the boot event.
 

Macros

#define sl_bt_evt_system_boot_id   0x000100a0
 Identifier of the boot event.
 

Detailed Description

Indicates that the device has started and the radio is ready.

This event carries the firmware build number and other software and hardware identification codes.


Data Structure Documentation

◆ sl_bt_evt_system_boot_s

struct sl_bt_evt_system_boot_s

Data structure of the boot event.

Data Fields
uint16_t major

Major release version

uint16_t minor

Minor release version

uint16_t patch

Patch release number

uint16_t build

Build number

uint32_t bootloader

Bootloader version

uint16_t hw

Hardware type

uint32_t hash

Version hash