sl_bt_evt_system_errorSystem
Indicates that an error has occurred.
Data Structures | |
struct | sl_bt_evt_system_error_s |
Data structure of the error event. | |
Macros | |
#define | sl_bt_evt_system_error_id 0x060100a0 |
Identifier of the error event. | |
Detailed Description
Indicates that an error has occurred.
See error codes table for more information.
Data Structure Documentation
◆ sl_bt_evt_system_error_s
struct sl_bt_evt_system_error_s |
Data structure of the error event.
Data Fields | ||
---|---|---|
uint16_t | reason |
Result code
|
uint8array | data |
Data related to the error; this field can be empty. |