Silicon Labs
bluetooth/3.3/general/firmware-upgrade/adding-gecko-bootloader-to-bluetooth-projects
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
      Results 1-5 of 5 for bluetooth/3.3/general/firmware-upgrade/adding-gecko-bootloader-to-bluetooth-projects in 0.23 seconds
      Uploading Firmware Images Using OTA DFU | Firmware Upgrade | Bluetooth LE | v3.1 | Silicon Labs
      https://docs.silabs.com/.../uploading-firmware-images-using-ota-...
      Home ... // Bluetooth LE//Version 3.1 //General //Firmware Upgrade //Uploading Firmware Images Using OTA DFU ... Gecko Bootloader can load application images into the application area from the ...
      Secure OTA DFU | Firmware Upgrade | Bluetooth Mesh | v7.0.2 | Silicon Labs
      https://docs.silabs.com/.../secure-ota-...
      Upgrade file authentication is only checked while upgrading. ... To restart the device in OTA mode, the following API is used: sl_bt_system_reset(2) is used.
      OTA | OTA | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/....
      // Bluetooth LE//Version 5.0 //API Reference ... The Apploader runs as a Bootloader communication plugin on series 2 and the Apploader ... Set the device name to be used during the OTA update.
      Using Bluetooth Security Features in Silicon Labs Bluetooth SDK | General Security | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../using-bluetooth-security-features-in-silicon-labs-bluetooth-...
      //General //General Security //Using Bluetooth Security Features in Silicon Labs ... Bluetooth uses AES-128 as the encryption algorithm ... To use the security features, do the following:
      GATT Server | GATT Server | Bluetooth LE | v3.2 | Silicon Labs
      https://docs.silabs.com/....
      See UG118: Blue Gecko Bluetooth Profile Toolkit Developer's Guide for how to declare capabilities in the GATT database. ... See Bluetooth specification Vol 3, Part G, 7.2 for the values.
        Results 1-5 of 5 for bluetooth/3.3/general/firmware-upgrade/adding-gecko-bootloader-to-bluetooth-projects