Security Manager#

Security Manager.

Modules

Security Manager configuration flags

sl_bt_evt_sm_passkey_display

Indicates a request to display the passkey to the user.

sl_bt_evt_sm_passkey_request

Indicates a request for the passkey prompt displayed on the remote device.

sl_bt_evt_sm_confirm_passkey

Indicates a request for passkey display and confirmation by the user.

sl_bt_evt_sm_bonded

Triggered after the pairing or bonding procedure is successfully completed.

sl_bt_evt_sm_bonding_failed

This event is triggered if the pairing or bonding procedure fails.

sl_bt_evt_sm_confirm_bonding

Indicates a user request to display that the new bonding request is received and for the user to confirm the request.

Enumerations

enum  

sl_bt_sm_io_capability_t { sl_bt_sm_io_capability_displayonly = 0x0, sl_bt_sm_io_capability_displayyesno = 0x1, sl_bt_sm_io_capability_keyboardonly = 0x2, sl_bt_sm_io_capability_noinputnooutput = 0x3, sl_bt_sm_io_capability_keyboarddisplay = 0x4 }

These values define the security management related I/O capabilities supported by the device.

Functions

sl_status_t 

sl_bt_sm_configure (uint8_t flags, uint8_t io_capabilities)

sl_status_t 

sl_bt_sm_set_minimum_key_size (uint8_t minimum_key_size)

sl_status_t 

sl_bt_sm_set_debug_mode ()

sl_status_t 

sl_bt_sm_add_to_whitelist (bd_addr address, uint8_t address_type)

sl_status_t 

sl_bt_sm_store_bonding_configuration (uint8_t max_bonding_count, uint8_t policy_flags)

sl_status_t 

sl_bt_sm_set_bondable_mode (uint8_t bondable)

sl_status_t 

sl_bt_sm_set_passkey (int32_t passkey)

sl_status_t 

sl_bt_sm_increase_security (uint8_t connection)

sl_status_t 

sl_bt_sm_enter_passkey (uint8_t connection, int32_t passkey)

sl_status_t 

sl_bt_sm_passkey_confirm (uint8_t connection, uint8_t confirm)

sl_status_t 

sl_bt_sm_bonding_confirm (uint8_t connection, uint8_t confirm)

sl_status_t 

sl_bt_sm_delete_bonding (uint8_t bonding)

sl_status_t 

sl_bt_sm_delete_bondings ()

sl_status_t 

sl_bt_sm_get_bonding_handles (uint32_t reserved, uint32_t *num_bondings, size_t max_bondings_size, size_t *bondings_len, uint8_t *bondings)

sl_status_t 

sl_bt_sm_get_bonding_details (uint32_t bonding, bd_addr *address, uint8_t *address_type, uint8_t *security_mode, uint8_t *key_size)

sl_status_t 

sl_bt_sm_find_bonding_by_address (bd_addr address, uint32_t *bonding, uint8_t *security_mode, uint8_t *key_size)

sl_status_t 

sl_bt_sm_set_legacy_oob (uint8_t enable, aes_key_128 oob_data)

sl_status_t 

sl_bt_sm_set_oob (uint8_t enable, aes_key_128 *random, aes_key_128 *confirm)

sl_status_t 

sl_bt_sm_set_remote_oob (uint8_t enable, aes_key_128 random, aes_key_128 confirm)

Detailed Description#

Security Manager.

The commands in this class manage Bluetooth security, including commands for starting and stopping encryption and commands for management of all bonding operations.

Use the following procedure to bond with a remote device:

Use the following procedure to respond to the bonding initiated by a remote device:

  • Use the command sl_bt_sm_configure to configure security requirements and I/O capabilities of this device.

  • Use the command sl_bt_sm_set_bondable_mode to set this device into bondable mode.

  • Use the command sl_bt_advertiser_start to start connectable advertising.

  • Open a connection to this device from the remote device.

  • After the connection is open, start the bonding process on the remote device.

If MITM is required, the application needs to display or ask the user to enter a passkey during the process. See events sl_bt_evt_sm_passkey_display and sl_bt_evt_sm_passkey_request for more information.

Enumeration Type Documentation#

◆sl_bt_sm_io_capability_t#

enum sl_bt_sm_io_capability_t

These values define the security management related I/O capabilities supported by the device.

Enumerator

sl_bt_sm_io_capability_displayonly 

(0x0) Display Only

sl_bt_sm_io_capability_displayyesno 

(0x1) Display with Yes/No-buttons

sl_bt_sm_io_capability_keyboardonly 

(0x2) Keyboard Only

sl_bt_sm_io_capability_noinputnooutput 

(0x3) No Input and No Output

sl_bt_sm_io_capability_keyboarddisplay 

(0x4) Display with Keyboard

Function Documentation#

◆sl_bt_sm_configure()#

sl_status_t sl_bt_sm_configure

(

uint8_t 

flags,

uint8_t 

io_capabilities

)

Configure security requirements and I/O capabilities of the system.

Parameters

[in]

flags

Security requirement flags. This value can be a bitmask of multiple flags from Security Manager configuration flags

Bit 0:* 0: Allow bonding without authentication

  • 1: Bonding requires authentication (Man-in-the-Middle protection)

Bit 1:* 0: Allow encryption without bonding

  • 1: Encryption requires bonding. Note that this setting will also enable bonding.

Bit 2:* 0: Allow bonding with legacy pairing

  • 1: Secure connections only

Bit 3:* 0: Bonding request does not need to be confirmed

Bit 4:* 0: Allow all connections

  • 1: Allow connections only from bonded devices

Bit 5:* 0: Prefer just works pairing when both options are possible based on the settings.

  • 1: Prefer authenticated pairing when both options are possible based on the settings.

Bit 6:* 0: Allow secure connections OOB pairing with OOB data from only one device.

  • 1: Require secure connections OOB data from both devices.

Bit 7: Reserved Default value: 0x00

[in]

io_capabilities

Enum sl_bt_sm_io_capability_t. I/O Capabilities. The default I/O Capability used by the stack is No Input and No Output. Values:

  • sl_bt_sm_io_capability_displayonly (0x0): Display Only

  • sl_bt_sm_io_capability_displayyesno (0x1): Display with Yes/No-buttons

  • sl_bt_sm_io_capability_keyboardonly (0x2): Keyboard Only

  • sl_bt_sm_io_capability_noinputnooutput (0x3): No Input and No Output

  • sl_bt_sm_io_capability_keyboarddisplay (0x4): Display with Keyboard

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_set_minimum_key_size()#

sl_status_t sl_bt_sm_set_minimum_key_size

(

uint8_t 

minimum_key_size

)

Set the minimum allowed key size used for bonding. The default value is 16 bytes.

Parameters

[in]

minimum_key_size

Minimum allowed key size for bonding. Range: 7 to 16

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_set_debug_mode()#

sl_status_t sl_bt_sm_set_debug_mode

(

)

Set Security Manager in debug mode. In this mode, the secure connections bonding uses known debug keys, so that the encrypted packet can be opened by Bluetooth protocol analyzer. To disable the debug mode, restart the device.

Bondings made in debug mode are unsecure.

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_add_to_whitelist()#

sl_status_t sl_bt_sm_add_to_whitelist

(

bd_addr

address,

uint8_t 

address_type

)

Add device to accept list, which can be enabled with sl_bt_gap_enable_whitelisting.

Parameters

[in]

address

Address of the device added to accept list

[in]

address_type

Address type of the device added to accept list. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_store_bonding_configuration()#

sl_status_t sl_bt_sm_store_bonding_configuration

(

uint8_t 

max_bonding_count,

uint8_t 

policy_flags

)

Set the maximum allowed bonding count and bonding policy. The maximum number of bondings that can be supported depends on how much user data is stored in the NVM and the NVM size. When bond policy value 1 or 2 is selected, the stack will automatically write the new bond, as per the policy, only if the maximum allowed bonding count has been reached. If the stack can't write a new bond for any other reason (e.g., NVM is full), an error will be thrown through the bonding_failed event indicating why the bonding was not written. The application has to manually release space from the NVM (e.g., by deleting one of the existing bonds or application data) so that a new bond can be saved. The default value is 13.

Parameters

[in]

max_bonding_count

Maximum allowed bonding count. Range: 1 to 32

[in]

policy_flags

Bonding policy. Values:

  • 0: If database is full, new bonding attempts will fail

  • 1: New bonding will overwrite the oldest existing bonding

  • 2: New bonding will overwrite the bonding that was used the longest time ago

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_set_bondable_mode()#

sl_status_t sl_bt_sm_set_bondable_mode

(

uint8_t 

bondable

)

Set whether the device should accept new bondings. By default, the device does not accept new bondings.

Parameters

[in]

bondable

Bondable mode. Values:

  • 0: New bondings not accepted

  • 1: Bondings allowed

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_set_passkey()#

sl_status_t sl_bt_sm_set_passkey

(

int32_t 

passkey

)

Enter a fixed passkey, which will be used in the sl_bt_evt_sm_passkey_display event.

Parameters

[in]

passkey

Passkey. Valid range: 0-999999. Set -1 to disable and start using random passkeys.

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_increase_security()#

sl_status_t sl_bt_sm_increase_security

(

uint8_t 

connection

)

Enhance the security of a connection to current security requirements. On an unencrypted connection, it will encrypt the connection and will also perform bonding if requested by both devices. On an encrypted connection, it will cause the connection to be re-encrypted.

Parameters

[in]

connection

Connection handle

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

  • sl_bt_evt_connection_parameters - Triggered after increasing security has been completed successfully and indicates the latest security mode of the connection.

  • sl_bt_evt_sm_bonded - Triggered if pairing or bonding was performed in this operation and the result is successful.

  • sl_bt_evt_sm_bonding_failed - Triggered if pairing or bonding was performed in this operation and the result has failed.

◆sl_bt_sm_enter_passkey()#

sl_status_t sl_bt_sm_enter_passkey

(

uint8_t 

connection,

int32_t 

passkey

)

Enter a passkey after receiving a passkey request event.

Parameters

[in]

connection

Connection handle

[in]

passkey

Passkey. Valid range: 0-999999. Set -1 to cancel pairing.

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_passkey_confirm()#

sl_status_t sl_bt_sm_passkey_confirm

(

uint8_t 

connection,

uint8_t 

confirm

)

Accept or reject the reported passkey confirm value.

Parameters

[in]

connection

Connection handle

[in]

confirm

Acceptance. Values:

  • 0: Reject

  • 1: Accept confirm value

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_bonding_confirm()#

sl_status_t sl_bt_sm_bonding_confirm

(

uint8_t 

connection,

uint8_t 

confirm

)

Accept or reject the bonding request.

Parameters

[in]

connection

Connection handle

[in]

confirm

Acceptance. Values:

  • 0: Reject

  • 1: Accept bonding request

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_delete_bonding()#

sl_status_t sl_bt_sm_delete_bonding

(

uint8_t 

bonding

)

Delete specified bonding information or accept list filtering from the persistent store.

Parameters

[in]

bonding

Bonding handle

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_delete_bondings()#

sl_status_t sl_bt_sm_delete_bondings

(

)

Delete all bonding information and accept list filtering from the persistent store. This will also delete device local identity resolving key (IRK).

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_get_bonding_handles()#

sl_status_t sl_bt_sm_get_bonding_handles

(

uint32_t 

reserved,

uint32_t * 

num_bondings,

size_t 

max_bondings_size,

size_t * 

bondings_len,

uint8_t * 

bondings

)

Get number of entries and bitmask of their handles saved in the bonding database. The entry in the bonding database can be either bonding or accept list filtering device.

To get the bonding type and peer device address of a bonding, use the sl_bt_sm_get_bonding_details command. The bonding handle can be calculated from the handle bitmask returned by this command, or alternatively, repeat calling the sl_bt_sm_get_bonding_details command to get the detailed information of all bondings.

Parameters

[in]

reserved

Use the value 0 on this reserved field. Do not use none-zero values because they are reserved for future use.

[out]

num_bondings

Total number of bondings and accept list filtering devices stored in bonding database.

[in]

max_bondings_size

Size of output buffer passed in bondings

[out]

bondings_len

On return, set to the length of output data written to bondings

[out]

bondings

4 byte bit field of used bonding handles in little endian format. Bit 0 of first byte is bonding handle 0, bit 0 of second byte is bonding handle 8 etc. If the bit is 1 that bonding handle exists in the bonding database.

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_get_bonding_details()#

sl_status_t sl_bt_sm_get_bonding_details

(

uint32_t 

bonding,

bd_addr * 

address,

uint8_t * 

address_type,

uint8_t * 

security_mode,

uint8_t * 

key_size

)

Get the detailed information for a bonding entry. Data includes remote device address and address type as well as security mode for bonding and a used encryption key length.

To get the detailed information of all bondings, repeat calling this command starting from 0 as the bonding handle value until the maximum number of configured bondings are reached. Use 32 as the maximum number if the configured number is unknown.

Parameters

[in]

bonding

Bonding handle

[out]

address

Bluetooth address of the remote device

[out]

address_type

Address type. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

[out]

security_mode

Connection security mode. Accept list filtering entry has security mode as no security. Values:

  • sl_bt_connection_mode1_level1 (0x0): No security

  • sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption

  • sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption

  • sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key

[out]

key_size

Key length in bytes, 0 for accept list filtering entry

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_find_bonding_by_address()#

sl_status_t sl_bt_sm_find_bonding_by_address

(

bd_addr

address,

uint32_t * 

bonding,

uint8_t * 

security_mode,

uint8_t * 

key_size

)

Find the bonding or accept list filtering entry by using a Bluetooth device address.

Parameters

[in]

address

The Bluetooth device address

[out]

bonding

The bonding handle

[out]

security_mode

Connection security mode. Accept list filtering entry has security mode as no security. Values:

  • sl_bt_connection_mode1_level1 (0x0): No security

  • sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption

  • sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption

  • sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key

[out]

key_size

Key length in bytes, 0 for accept list filtering entry

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_set_legacy_oob()#

sl_status_t sl_bt_sm_set_legacy_oob

(

uint8_t 

enable,

aes_key_128

oob_data

)

Set Out-Of-Band (OOB) encryption data for a legacy pairing of a device. OOB data may be, for example, a PIN code exchanged over an alternate path, such as NFC. The device will not allow any other bonding if OOB data is set. OOB data can't be set simultaneously with secure connections OOB data.

Parameters

[in]

enable

Enable OOB with legacy pairing. Values:

  • 0: disable

  • 1: enable

[in]

oob_data

16-byte legacy pairing OOB data in little endian format.

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_set_oob()#

sl_status_t sl_bt_sm_set_oob

(

uint8_t 

enable,

aes_key_128 * 

random,

aes_key_128 * 

confirm

)

Enable the use of Out-Of-Band (OOB) encryption data for a device for secure connections pairing. Enabling will generate new OOB data and confirm values, which can be sent to the remote device. After enabling the secure connections OOB data, the remote devices OOB data can be set with sl_bt_sm_set_remote_oob. Calling this function will erase any set remote device OOB data and confirm values. The device will not allow any other bonding if OOB data is set. The secure connections OOB data cannot be enabled simultaneously with legacy pairing OOB data.

Parameters

[in]

enable

Enable OOB with secure connections pairing. Values:

  • 0: disable

  • 1: enable

[out]

random

16-byte randomly-generated secure connections OOB data in little endian format.

[out]

confirm

16-byte confirm value for the OOB random value in little endian format.

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_sm_set_remote_oob()#

sl_status_t sl_bt_sm_set_remote_oob

(

uint8_t 

enable,

aes_key_128

random,

aes_key_128

confirm

)

Set Out-Of-Band (OOB) data and confirm values received from the remote device for secure connections pairing. OOB data must be enabled with sl_bt_sm_set_oob before setting the remote device OOB data.

Parameters

[in]

enable

Enable remote device OOB data with secure connections pairing. Values:

  • 0: disable

  • 1: enable

[in]

random

16-byte remote device secure connections OOB data in little endian format.

[in]

confirm

16-byte remote device confirm value for the OOB random value in little endian format.

ReturnsSL_STATUS_OK if successful. Error code otherwise.