Sync PAST#
Sync PAST.
Functions | |
sl_status_t | sl_bt_sync_past_transfer (uint8_t connection, uint16_t service_data, uint16_t sync) |
Detailed Description#
Sync PAST.
Transfer the synchronization information of a synchronized periodic advertising train to a remote device using Periodic Advertising Synchronization Transfer (PAST) over a connection.
Function Documentation#
◆sl_bt_sync_past_transfer()#
sl_status_t sl_bt_sync_past_transfer | ( | uint8_t |
|
uint16_t |
| ||
uint16_t |
| ||
) |
Transfer the synchronization information of a periodic advertising train for which a sync has been established.
Parameters
[in] |
| Connection handle of the connection used to transmit the sync transfer |
[in] |
| A value provided by the application for use by the peer device. |
[in] |
| Handle of the periodic advertising synchronization to transfer |
ReturnsSL_STATUS_OK if successful. Error code otherwise.