Testing Commands#
Testing Commands.
Modules |
Indicates that the radio has processed a test start or end command. |
Enumerations | |
enum | sl_bt_test_packet_type_t { sl_bt_test_pkt_prbs9 = 0x0, sl_bt_test_pkt_11110000 = 0x1, sl_bt_test_pkt_10101010 = 0x2, sl_bt_test_pkt_11111111 = 0x4, sl_bt_test_pkt_00000000 = 0x5, sl_bt_test_pkt_00001111 = 0x6, sl_bt_test_pkt_01010101 = 0x7, sl_bt_test_pkt_pn9 = 0xfd, sl_bt_test_pkt_carrier = 0xfe } |
Test packet types supported by the stack. | |
enum | sl_bt_test_phy_t { sl_bt_test_phy_1m = 0x1, sl_bt_test_phy_2m = 0x2, sl_bt_test_phy_125k = 0x3, sl_bt_test_phy_500k = 0x4 } |
Test PHY types. |
Functions | |
sl_status_t | sl_bt_test_dtm_tx_v4 (uint8_t packet_type, uint8_t length, uint8_t channel, uint8_t phy, int8_t power_level) |
sl_status_t | sl_bt_test_dtm_tx_cw (uint8_t packet_type, uint8_t channel, uint8_t phy, int16_t power_level) |
sl_status_t | sl_bt_test_dtm_rx (uint8_t channel, uint8_t phy) |
sl_status_t |
Detailed Description#
Testing Commands.
Enumeration Type Documentation#
◆sl_bt_test_packet_type_t#
Test packet types supported by the stack.
Enumerator | |
|---|---|
sl_bt_test_pkt_prbs9 | (0x0) PRBS9 packet payload |
sl_bt_test_pkt_11110000 | (0x1) 11110000 packet payload |
sl_bt_test_pkt_10101010 | (0x2) 10101010 packet payload |
sl_bt_test_pkt_11111111 | (0x4) 11111111 packet payload |
sl_bt_test_pkt_00000000 | (0x5) 00000000 packet payload |
sl_bt_test_pkt_00001111 | (0x6) 00001111 packet payload |
sl_bt_test_pkt_01010101 | (0x7) 01010101 packet payload |
sl_bt_test_pkt_pn9 | (0xfd) PN9 continuously modulated output |
sl_bt_test_pkt_carrier | (0xfe) Unmodulated carrier |
◆sl_bt_test_phy_t#
enum sl_bt_test_phy_t |
Test PHY types.
Enumerator | |
|---|---|
sl_bt_test_phy_1m | (0x1) 1M PHY |
sl_bt_test_phy_2m | (0x2) 2M PHY |
sl_bt_test_phy_125k | (0x3) 125k Coded PHY |
sl_bt_test_phy_500k | (0x4) 500k Coded PHY |
Function Documentation#
◆sl_bt_test_dtm_tx_v4()#
sl_status_t sl_bt_test_dtm_tx_v4 | ( | uint8_t |
|
uint8_t |
| ||
uint8_t |
| ||
uint8_t |
| ||
int8_t |
| ||
) |
Start a transmitter test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.
In the transmitter test, the device sends packets continuously with a fixed interval. The type and length of each packet is set by packet_type and length parameters. The parameter phy specifies which PHY is used to transmit the packets. All devices support at least 1M PHY. A special packet type, test_pkt_carrier , can be used to transmit continuous unmodulated carrier. The length field is ignored in this mode. As this command has the limitation within the value of power_level, use of sl_bt_test_dtm_tx_cw for custom waves is recommended.
Stop the test using the sl_bt_test_dtm_end command.
Parameters
[in] |
| Packet type to transmit. Values:
|
[in] |
| Packet length in bytes
|
[in] |
| Bluetooth channel
|
[in] |
| PHY to use. Values:
|
[in] |
| TX power level in unit dBm. Values:
|
ReturnsCommand result Events
sl_bt_evt_test_dtm_completed - This event is received when the command is processed.
◆sl_bt_test_dtm_tx_cw()#
sl_status_t sl_bt_test_dtm_tx_cw | ( | uint8_t |
|
uint8_t |
| ||
uint8_t |
| ||
int16_t |
| ||
) |
Start a transmitter test for a custom wave. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.
In the custom wave transmitter test, the device continuously transmits the career. The parameter packet_type specifies the packet type. The parameter phy specifies which PHY is used to transmit the packets. All devices support at least 1M PHY.
Stop the test using the sl_bt_test_dtm_end command.
Parameters
[in] |
| Packet type to transmit. Values:
|
[in] |
| Bluetooth channel
|
[in] |
| PHY to use. Values:
|
[in] |
| TX power level. Unit: 0.1 dBm. |
If the value exceeds the range of power level value, allowed by the device, the command will adjust the power level to the closest minimum or maximum value. |
ReturnsCommand result Events
sl_bt_evt_test_dtm_completed - This event is received when the command is processed.
◆sl_bt_test_dtm_rx()#
sl_status_t sl_bt_test_dtm_rx | ( | uint8_t |
|
uint8_t |
| ||
) |
Start a receiver test against a separate Bluetooth tester device. When the command is processed by the radio, a sl_bt_evt_test_dtm_completed event is triggered. This event indicates whether the test started successfully.
Parameter phy specifies which PHY is used to receive the packets. All devices support at least 1M PHY.
The test may be stopped using sl_bt_test_dtm_end command. This will trigger another sl_bt_evt_test_dtm_completed event, which carries the number of packets received during the test.
Parameters
[in] |
| Bluetooth channel
|
[in] |
| PHY to use. Values:
|
ReturnsCommand result Events
sl_bt_evt_test_dtm_completed - This event is received when the command is processed.
◆sl_bt_test_dtm_end()#
sl_status_t sl_bt_test_dtm_end | ( | ) |
End a transmitter or a receiver test. When the command is processed by the radio and the test has ended, a sl_bt_evt_test_dtm_completed event is triggered.
ReturnsCommand result Events
sl_bt_evt_test_dtm_completed - Received when the command is processed by the radio and the test has ended.