Bluetooth functions in the 2.4 GHz frequency range. ... Channel map update procedure is part of the Bluetooth 4.0 specification. ... Bluetooth Low Energy has two channel selection algorithms.
Training ... Register // Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... 3: Advertise on CH37 and CH38 4: Advertise on CH39 5: Advertise on CH37 and CH39
// Bluetooth LE//Version 3.1 //General ... Because Bluetooth stack follows strict regulations, the maximum output power is 10 dBm in those cases when AFH is not enabled (or AFH is enabled but ...