Silicon Labs
bluetooth/5.0/data_types
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
      Results 1-5 of 5 for bluetooth/5.0/data_types in 0.20 seconds
      BGAPI | BGAPI headers | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/....
      // Bluetooth LE//Version 5.0 //API Reference ... Bits 0 - 2: Highest 3 bits of the data payload length field Bits 3 - 5: Device type Bit value 100: Bluetooth LE Bit value 101: Bluetooth Mesh
      sl_bt_evt_scanner_scan_reportScanner | Scanner | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../a00...
      // Bluetooth LE//Version 5.0 //API Reference ... Value 0 indicates no periodic advertising. ... Time range: 7.5 ms to 81.92 s | | uint8array | data | Advertising or scan response data |
      Event Type Flags of Advertisement ReportsScanner | Scanner | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../a00...
      Training ... // Bluetooth LE//Version 5.0 //API Reference ... #define SL_BT_SCANNER_EVENT_FLAG_CONNECTABLE 0x1 A connectable advertising data packet ◆SL_BT_SCANNER_EVENT_FLAG_SCANNABLE#
      Security Manager | Bluetooth Stack API Reference | Bluetooth LE | v7.1.1 | Silicon Labs
      https://docs.silabs.com/.../sl-bt...
      sl_bt_rsp_sm_set_bonding_data_id 0x1c0f0020 ... 0: If database is full, new bonding attempts will fail ... Data includes remote device address and address type as well as security mode for ...
      Creating an Eddystone-URL Beacon | Advertising & Scanning | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/....
      Training ... // Bluetooth LE//Version 2.13 // ... The Eddystone format defines four different packet types. ... gecko_cmd_le_gap_bt5_set_adv_data(0, 0, EDDYSTONE_DATA_LEN, eddystone_data)
        Results 1-5 of 5 for bluetooth/5.0/data_types