Silicon Labs
bluetooth/5.0/functions-vars-i
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
      Results 1-5 of 5 for bluetooth/5.0/functions-vars-i in 0.10 seconds
      Error codes | Error Codes | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/....
      // Bluetooth LE//Version 2.13 //API Reference //Error Codes You are viewing documentation for version: 2.13 ... error code indicates that an attempt to create a new ACL Connection to a
      Status Codes | API Documentation | Platform | v5.0.2 | Silicon Labs
      https://docs.silabs.com/.../sta...
      You are viewing documentation for version: 5.0.2 Status Codes# Status Codes contains error and status code definitions used by Simplicity SDK ... Bluetooth cannot be used on this hardware.
      Advertiser | Bluetooth Stack API Reference | Bluetooth LE | v8.0.0 | Silicon Labs
      https://docs.silabs.com/.../sl-bt-adverti...
      Training ... Register // Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... Wrong state error is returned if advertising has been enabled on the advertising set.
      Adaptive Frequency Hopping | System & Performance | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../adaptive-frequency-hopp...
      Bluetooth functions in the 2.4 GHz frequency range. ... Channel map update procedure is part of the Bluetooth 4.0 specification. ... Bluetooth Low Energy has two channel selection algorithms.
      TX Power Limitations for Regulatory Compliance (ETSI, FCC) | System & Performance | Bluetooth LE | v3.1 | Silicon Labs
      https://docs.silabs.com/.../tx-power-limitations-for-regulatory-compliance-etsi-...
      // Bluetooth LE//Version 3.1 //General ... Because Bluetooth stack follows strict regulations, the maximum output power is 10 dBm in those cases when AFH is not enabled (or AFH is enabled but ...
        Results 1-5 of 5 for bluetooth/5.0/functions-vars-i