// Platform//Version 5.0.1 //Security ... Devices with the SE subsystem includes a low level crypto API where the SE Manager will use the SE hardware peripherals to accelerate cryptographic ...
Configuration Options The API Flow Control Support Example ... ◆ UARTDRV_Status_t typedef uint32_t UARTDRV_Status_t A UART status return type. Bitfield of UARTDRV_STATUS_* values.
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-5 of 5 for bluetooth/5.0/general/security/using-bluetooth-security-features-in-silicon-labs-bluetooth-sdk