Silicon Labs
bluetooth/functions-vars-r
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
Results 1-5 of 5 for bluetooth/functions-vars-r in 0.16 seconds
Button API - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-but...
There is currently one type of button supported by the button driver: Simple Button Driver All button functions are called through the generic driver, which then references functions in ...
ProductMicrocontrollers Resource TypeSoftware API documentation
Simple Button Driver | API Documentation | Platform | v5.1.0 | Silicon Labs
https://docs.silabs.com/.../simple-but...
// Platform//Version 5.1.0 //Drivers //API Documentation //Button API //Simple Button Driver You are viewing documentation for version: ... BUTTON input capture using polling and debouncing.
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
Driver for the Bosch Sensortec BMP280 barometric pressure sensor ... Driver for the Invensense ICM20648 6-axis motion sensor ... Platform Services Detail Device Initialization
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
Login ... // Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible.
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
Training ... // Gecko Platform//Version 4.4.1 //Services ... This driver works with a configurable time unit called tick. ... All API functions can be called from within interrupt handlers.
    Results 1-5 of 5 for bluetooth/functions-vars-r