Handling Missing Bonding Keys

Description

This document describes two scenarios that can occur after a bond has been established between a smartphone and a Bluetooth-Capable EFR32.

Case 1: Bonding keys are deleted from the smartphone.

Case 2: Bonding keys are deleted from the EFR32.

As an introduction to Bluetooth Security features, read Using Bluetooth security features in Silicon Labs Bluetooth SDK.

Disclaimer: This document and the sample application attached with it is to be used for information, reference about the topic and testing. It is not in any way production ready code. The use of the code will be at your own risk.

Setting up

Master: A smartphone with the Blue Gecko app

  1. An Android smartphone (A Sony Xperia Z1 running Android 5.1.1 OS, doesn’t support LE secure connections)

  2. Another Android smartphone (A Samsung Galaxy S6 Edge running Android 7.0 OS, supports LE secure connections)

  3. An Apple smartphone (iPhone 6, running iOS 11.2.6 supports LE secure connections)

Slave: An EFR32 Radio board (a BGM module in this case, it supports LE secure connections) (Programmed with Bluetooth SDK 2.11)

  1. Create an soc-empty example project in Simplicity Studio for your specific radio board or OPN (in case you are on a custom design), using Bluetooth SDK 2.11 (GSDK 2.5) or above.

  2. The function code is in the app.c file. Copy and replace this file to the project folder.

  3. In app.h set #define DEBUG_LEVEL 1

  4. Import the gatt.xml into the project by following the instructions in UG365: GATT Configurator User’s Guide section 2.6

  5. Compile and flash. The output will be shown on the Serial Port.

Usage

The following are the most relevant BGAPI commands used in the sample code attached with this KBA.

gecko_cmd_sm_set_passkey(-1);

gecko_cmd_sm_configure(0x0B,sm_io_capability_displayonly);

gecko_cmd_sm_set_bondable_mode(1);

gecko_cmd_sm_increase_security(connectionhandle);

More details of all these commands can be found in Bluetooth API Reference guide.

Connecting

Android

According to our observation, Android OS treats pairing and connecting as two separate events. Pairing is optional if your GATT database does not contain any characteristic that requires encryption or bonding. You can connect, not pair and still be able to read and write other characteristics. A connection made between the EFR and Smartphone is security level 1. When paired, security level increases to 3 or 4 depending on Legacy or Secure connections respectively.

img

Figure 1: The Bluetooth Browser Showing the Empty Example Device

img

Figure 2: Connected but not Bonded to the EFR

img

Figure 3: Optional Pairing/Bonding Request Received

Apple

iOS actively asks for a pairing request if your GATT database contains any characteristic that require encryption or bonding because it reads all the characteristics as soon as you connect a device. As a result, you receive an active pairing request while setting up a connection. The request is initiated with security level 1 but is increased up to level 4 once a bond is created successfully.

img

Figure 4: Bluetooth Browser in iOS

img

Figure 5: Active Pairing/Bonding Request Received while Connecting

Observations

These observations are for the flags set to values as mentioned above. These will vary based on the values and device capabilities as mentioned in Using Bluetooth Security Features in Silicon Labs Bluetooth SDK.

Scenario 1: Bonding keys are lost on the smartphone.

iPhone: A new pairing request is initiated with a request to enter the passkey. Upon successful pairing, security Level_4 is achieved. The EFR overwrites the existing bonding keys.

Android (both test devices): Android phones receive two new pairing requests. The first one with a yes(pair)/no option to pair. The second one asks for a passkey entry. Upon successful pairing security Level_3 is achieved for phones which don’t support secure connections. Security Level_4 is achieved for phones which support secure pairing.

Scenario 2: Bonding keys are lost on the EFR.

  1. Android Blue Gecko App connecting to EFR

    a. On LE secure supported phones: Pairing fails for a reason

    0x0206: pin_or_key_missing; Pairing failed because of missing PIN, or authentication failed because of missing key. The connection remains open with security Level_1. This error can be caught, and an increase security function (sm_increase_security; refer section ) can be triggered. As a result, a passkey entry request is received on the phone. Upon successful pairing, security Level_4 is achieved.

    b. On phones which don’t support LE secure: Again, pairing fails for a reason

    0x0206: pin_or_key_missing; Pairing failed because of missing PIN, or authentication failed because of a missing key. The connection is terminated by the phone upon detecting a failed attempt and the bonding keys are deleted on the phone *. An error code 0x0213: remote user terminated is received. A repeated pairing attempt sets up new bonding keys on both sides as if they are connecting for the first time.

​ * This behavior can change based on your phone/Android version and hardware configurations of your phone.

  1. iOS App connecting to EFR

    Pairing fails with an error code 0x0206 (Pin or key missing). The connection remains open with security Level_1. This error can be caught in the gecko_evt_sm_bonding_failed_id, and an increase security function can be triggered. This command fails because of a timeout with error code 0x0185after about 15-30 seconds. This error is caught and an increase security function gecko_cmd_sm_increase_security(connectionhandle) triggers a new passkey request. Upon successful pairing, security Level_4 is achieved.

Testing the Example

The sample application attached with this document demonstrates these mechanisms for handling missing bonding keys on both sides. Create the project following the instructions in the attached readme file and flash it to a WSTK. This example prints to the WSTK VCOM so connect a terminal to the WSTK's COM Port on your PC to see the messages.

  1. Connect to the EFR32 named "Empty Example" from the Blue Gecko App Bluetooth Browser. Enter the passkey displayed on the console when asked.

  2. Disconnect. Delete bonding data from your phone settings> Bluetooth. Reconnect from the app. Note the observations on the serial monitor.

  3. Press reset on EFR32. The sample application attached with this KBA is designed to delete the bonding keys when you reset. IT IS NOT RECOMMENDED IN REAL APPLICATIONS. Follow step 1.

  4. Disconnect, press reset on EFR32, and reconnect (do not delete bonding data on the phone this time). Note the observations on the serial monitor.

Contribution credit: The example code attached with this KBA is based on the work of Théo Meyer from www.strataggem.com

Source