Network Protocol Data Unit.

Public Attributes#

uint8_t

Least significant bit of IV Index.

uint8_t

Network Identifier.

uint8_t

Network Control.

uint8_t

Time To Live.

uint32_t

Sequence number.

uint16_t

Source address.

uint16_t

Destination address.

size_t

Length of the Transport PDU.

const uint8_t *

Transport Protocol Data Unit.

size_t

Length of the NetMIC.

const uint8_t *

Pointer to the NetMIC data.

Public Attribute Documentation#

ivi#

uint8_t net_pdu_t::ivi

Least significant bit of IV Index.


nid#

uint8_t net_pdu_t::nid

Network Identifier.


ctl#

uint8_t net_pdu_t::ctl

Network Control.


ttl#

uint8_t net_pdu_t::ttl

Time To Live.


seq#

uint32_t net_pdu_t::seq

Sequence number.


src#

uint16_t net_pdu_t::src

Source address.


dst#

uint16_t net_pdu_t::dst

Destination address.


trans_pdu_len#

size_t net_pdu_t::trans_pdu_len

Length of the Transport PDU.


transport_pdu#

const uint8_t* net_pdu_t::transport_pdu

Transport Protocol Data Unit.


net_mic_len#

size_t net_pdu_t::net_mic_len

Length of the NetMIC.


net_mic#

const uint8_t* net_pdu_t::net_mic

Pointer to the NetMIC data.