Bluetooth Mesh message decoder library configuration.

License#

Copyright 2024 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.

  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.

  3. This notice may not be removed or altered from any source distribution.

/***************************************************************************/
#ifndef SL_BTMESH_DECODER_CONFIG_H
#define SL_BTMESH_DECODER_CONFIG_H

#define DECODE_FRIENDSHIP (1)

#define DECODE_DIRECTED_FORWARDING (1)

#define MAX_KEYS (16)

#define MAX_REASSEMBLER_COUNT (16)

#if DECODE_FRIENDSHIP

#define MAX_INCOMPLETE_FRIENDSHIP_COUNT (16)

#endif

#define MAX_VIRTUAL_LABELS (16)

#define SL_MESH_SENSOR_ARRAY_SIZE (10)

#define MAX_ADV_DATA_NUM            16

#endif // SL_BTMESH_DECODER_CONFIG_H

Macros#

#define

Whether to handle friendship messaging or not

#define

Whether to handle directed forwarding or not

#define

Maximum number of cryptographic keys (network keys, application keys, device keys, and friendship key material) that can be in use at any given time. The more keys are configured, the higher the runtime memory requirements.

Note that the PSA cryptographic library can limit the number of keys that exist concurrently, and there are multiple key derivations made for every network key and ongoing friendship. Moreover, there are multiple key derivations made for ongoing friendships.

#define

Maximum number of segmented message reassemblies that can be tracked in parallel. The more ressemblers are configured, the higher the runtime memory requirements.

#define

Maximum number of pending friendship establishments that can be tracked in parallel. The more pending friendships are configured, the higher the runtime memory requirements.

#define

Maximum number of Label UUIDs for virtual addresses. The more lavels are configured, the higher the runtime memory requirements.

#define

Maximum number of sensor data entries that can be stored during decoding.

#define

Maximum number of advertisement data fields

Macro Definition Documentation#

DECODE_FRIENDSHIP#

#define DECODE_FRIENDSHIP
Value:
(1)

Whether to handle friendship messaging or not


DECODE_DIRECTED_FORWARDING#

#define DECODE_DIRECTED_FORWARDING
Value:
(1)

Whether to handle directed forwarding or not


MAX_KEYS#

#define MAX_KEYS
Value:
(16)

Maximum number of cryptographic keys (network keys, application keys, device keys, and friendship key material) that can be in use at any given time. The more keys are configured, the higher the runtime memory requirements.

Note that the PSA cryptographic library can limit the number of keys that exist concurrently, and there are multiple key derivations made for every network key and ongoing friendship. Moreover, there are multiple key derivations made for ongoing friendships.


MAX_REASSEMBLER_COUNT#

#define MAX_REASSEMBLER_COUNT
Value:
(16)

Maximum number of segmented message reassemblies that can be tracked in parallel. The more ressemblers are configured, the higher the runtime memory requirements.


MAX_INCOMPLETE_FRIENDSHIP_COUNT#

#define MAX_INCOMPLETE_FRIENDSHIP_COUNT
Value:
(16)

Maximum number of pending friendship establishments that can be tracked in parallel. The more pending friendships are configured, the higher the runtime memory requirements.


MAX_VIRTUAL_LABELS#

#define MAX_VIRTUAL_LABELS
Value:
(16)

Maximum number of Label UUIDs for virtual addresses. The more lavels are configured, the higher the runtime memory requirements.


SL_MESH_SENSOR_ARRAY_SIZE#

#define SL_MESH_SENSOR_ARRAY_SIZE
Value:
(10)

Maximum number of sensor data entries that can be stored during decoding.


MAX_ADV_DATA_NUM#

#define MAX_ADV_DATA_NUM
Value:
16

Maximum number of advertisement data fields