Co-Processors (NCP and RCP)#
The Silicon Labs Bluetooth stack provides multiple APIs for the developer to access the Bluetooth functionality. Three modes are supported:
Standalone mode, where both the Bluetooth stack and the application run in an EFR32SoC or module. The application can be developed with C programming language.
Network Co-Processor (NCP) mode, where the Bluetooth stack runs in an EFR32 and the application runs on a separate host MCU. For this use case, the Bluetooth stack can be configured into NCP mode where the API is exposed over a serial interface such as UART.
Radio Co-Processor (RCP) mode, where only the Link Layer of the Bluetooth stack runs on the EFR32, and the Host Layer of the stack, as well as the application, runs on a separate host MCU or PC. In this use case, the Host Layer is developed by a third party, since Silicon Labs’ Bluetooth stack is only built for EFR32 SoCs / modules. The Link Layer and the host layer communicate via HCI (Host-Controller Interface), which is a standard interface between the two layers. The HCI can be accessed via UART following the Bluetooth SIG's UART (H4) transport protocol.
This section provides additional detail on the last two.
Using the Bluetooth Stack in Network Co-Processor Mode: Describes how to configure the NCP target and how to program the NCP host when using the Bluetooth Stack in Network Co-Processor mode
Enabling a Radio Co-Processor using the Bluetooth Controller and HCI Functions: Gives a short overview of the standard Host Controller Interface (HCI) and how to use it with a Silicon Labs Bluetooth LE controller.