Data Structures

Here are the data structures with brief descriptions:
ARM_CAN_CAPABILITIESCAN Device Driver Capabilities
ARM_CAN_MSG_INFOCAN Message Information
ARM_CAN_OBJ_CAPABILITIESCAN Object Capabilities
ARM_CAN_STATUSCAN Status
ARM_DRIVER_CANAccess structure of the CAN Driver
ARM_DRIVER_ETH_MACAccess structure of the Ethernet MAC Driver
ARM_DRIVER_ETH_PHYAccess structure of the Ethernet PHY Driver
ARM_DRIVER_FLASHAccess structure of the Flash Driver
ARM_DRIVER_I2CAccess structure of the I2C Driver
ARM_DRIVER_MCIAccess structure of the MCI Driver
ARM_DRIVER_NANDAccess structure of the NAND Driver
ARM_DRIVER_SAIAccess structure of the SAI Driver
ARM_DRIVER_SPIAccess structure of the SPI Driver
ARM_DRIVER_STORAGE
ARM_DRIVER_USARTAccess structure of the USART Driver
ARM_DRIVER_USBDAccess structure of the USB Device Driver
ARM_DRIVER_USBHAccess structure of USB Host Driver
ARM_DRIVER_USBH_HCIAccess structure of USB Host HCI (OHCI/EHCI) Driver
ARM_DRIVER_VERSIONDriver Version
ARM_ETH_LINK_INFOEthernet link information
ARM_ETH_MAC_ADDREthernet MAC Address
ARM_ETH_MAC_CAPABILITIESEthernet MAC Capabilities
ARM_ETH_MAC_TIMEEthernet MAC Time
ARM_FLASH_CAPABILITIESFlash Driver Capabilities
ARM_FLASH_INFOFlash information
ARM_FLASH_SECTORFlash Sector information
ARM_FLASH_STATUSFlash Status
ARM_I2C_CAPABILITIESI2C Driver Capabilities
ARM_I2C_STATUSI2C Status
ARM_MCI_CAPABILITIESMCI Driver Capabilities
ARM_MCI_STATUSMCI Status
ARM_NAND_CAPABILITIESNAND Driver Capabilities
ARM_NAND_ECC_INFONAND ECC (Error Correction Code) Information
ARM_NAND_STATUSNAND Status
ARM_SAI_CAPABILITIESSAI Driver Capabilities
ARM_SAI_STATUSSAI Status
ARM_SPI_CAPABILITIESSPI Driver Capabilities
ARM_SPI_STATUSSPI Status
ARM_STORAGE_BLOCKA storage block is a range of memory with uniform attributes
ARM_STORAGE_BLOCK_ATTRIBUTESAttributes of the storage range within a storage block
ARM_STORAGE_CAPABILITIESStorage Driver API Capabilities
ARM_STORAGE_INFO
ARM_STORAGE_SECURITY_FEATURES
ARM_STORAGE_STATUSOperating status of the storage controller
ARM_USART_CAPABILITIESUSART Device Driver Capabilities
ARM_USART_MODEM_STATUSUSART Modem Status
ARM_USART_STATUSUSART Status
ARM_USBD_CAPABILITIESUSB Device Driver Capabilities
ARM_USBD_STATEUSB Device State
ARM_USBH_CAPABILITIESUSB Host Driver Capabilities
ARM_USBH_HCI_CAPABILITIESUSB Host HCI (OHCI/EHCI) Driver Capabilities
ARM_USBH_PORT_STATEUSB Host Port State