CAN Object EventsCAN Interface

Callback objects events notified via ARM_CAN_SignalObjectEvent.

Macros

#define ARM_CAN_EVENT_SEND_COMPLETE   (1UL << 0)
 Send complete.
 
#define ARM_CAN_EVENT_RECEIVE   (1UL << 1)
 Message received.
 
#define ARM_CAN_EVENT_RECEIVE_OVERRUN   (1UL << 2)
 Received message overrun.
 

Description

Callback objects events notified via ARM_CAN_SignalObjectEvent.

The CAN driver generates callback objects events that are notified via the function ARM_CAN_SignalObjectEvent.

The following callback notification object events are generated:

Macro Definition Documentation

#define ARM_CAN_EVENT_SEND_COMPLETE   (1UL << 0)

Send complete.

See Also
ARM_CAN_SignalObjectEvent
#define ARM_CAN_EVENT_RECEIVE   (1UL << 1)

Message received.

See Also
ARM_CAN_SignalObjectEvent
#define ARM_CAN_EVENT_RECEIVE_OVERRUN   (1UL << 2)

Received message overrun.

See Also
ARM_CAN_SignalObjectEvent