Flash EventsFlash Interface

The Flash driver generates call back events that are notified via the function ARM_Flash_SignalEvent.

Macros

#define ARM_FLASH_EVENT_READY   (1UL << 0)
 Flash Ready.
 
#define ARM_FLASH_EVENT_ERROR   (1UL << 1)
 Read/Program/Erase Error.
 

Description

The Flash driver generates call back events that are notified via the function ARM_Flash_SignalEvent.

This section provides the event values for the ARM_Flash_SignalEvent callback function.

The following call back notification events are generated:

Macro Definition Documentation

#define ARM_FLASH_EVENT_READY   (1UL << 0)

Flash Ready.

#define ARM_FLASH_EVENT_ERROR   (1UL << 1)

Read/Program/Erase Error.