SPI Control CodesSPI Interface

Many parameters of the SPI driver are configured using the ARM_SPI_Control function.

Content

SPI Mode Controls
Specifies SPI mode.
 
SPI Frame Format
Defines the frame format.
 
SPI Data Bits
Defines the number of data bits.
 
SPI Bit Order
Defines the bit order.
 
SPI Slave Select Mode
Specifies SPI slave select mode.
 
SPI Miscellaneous Controls
Specifies additional miscellaneous controls.
 

Description

Many parameters of the SPI driver are configured using the ARM_SPI_Control function.

The various SPI control codes define:

Refer to the ARM_SPI_Control function for further details.