USBD Endpoint EventsUSB Device Interface
The USB Device driver generates Endpoint call back events that are notified via the function ARM_USBD_SignalEndpointEvent.
Macros | |
#define | ARM_USBD_EVENT_SETUP (1UL << 0) |
SETUP Packet. | |
#define | ARM_USBD_EVENT_OUT (1UL << 1) |
OUT Packet(s) | |
#define | ARM_USBD_EVENT_IN (1UL << 2) |
IN Packet(s) | |
Description
The USB Device driver generates Endpoint call back events that are notified via the function ARM_USBD_SignalEndpointEvent.
This section provides the event values for the ARM_USBD_SignalEndpointEvent callback function.
The following call back notification events are generated:
Macro Definition Documentation
#define ARM_USBD_EVENT_SETUP (1UL << 0) |
SETUP Packet.
#define ARM_USBD_EVENT_OUT (1UL << 1) |
OUT Packet(s)
#define ARM_USBD_EVENT_IN (1UL << 2) |
IN Packet(s)