NAND Control CodesNAND Interface

Many parameters of the NAND driver are configured using the ARM_NAND_Control function.

Content

NAND Mode Controls
Specify operation modes of the NAND interface.
 
NAND Bus Modes
Specify bus mode of the NAND interface.
 
NAND Data Bus Width
Specify data bus width of the NAND interface.
 
NAND Driver Strength
Specify driver strength of the NAND interface.
 

Description

Many parameters of the NAND driver are configured using the ARM_NAND_Control function.

Refer to the function ARM_NAND_Control for further details.