NAND Driver StrengthNAND Control Codes
Specify driver strength of the NAND interface.
Macros | |
#define | ARM_NAND_DRIVER_STRENGTH_18 (0x00) |
Driver Strength 2.0x = 18 Ohms. | |
#define | ARM_NAND_DRIVER_STRENGTH_25 (0x01) |
Driver Strength 1.4x = 25 Ohms. | |
#define | ARM_NAND_DRIVER_STRENGTH_35 (0x02) |
Driver Strength 1.0x = 35 Ohms (default) | |
#define | ARM_NAND_DRIVER_STRENGTH_50 (0x03) |
Driver Strength 0.7x = 50 Ohms. | |
Description
Specify driver strength of the NAND interface.
The defines can be used in the function ARM_NAND_Control for the parameter arg and with the ARM_NAND_DRIVER_STRENGTH as the control code.
Macro Definition Documentation
#define ARM_NAND_DRIVER_STRENGTH_18 (0x00) |
Driver Strength 2.0x = 18 Ohms.
#define ARM_NAND_DRIVER_STRENGTH_25 (0x01) |
Driver Strength 1.4x = 25 Ohms.
#define ARM_NAND_DRIVER_STRENGTH_35 (0x02) |
Driver Strength 1.0x = 35 Ohms (default)
#define ARM_NAND_DRIVER_STRENGTH_50 (0x03) |
Driver Strength 0.7x = 50 Ohms.