Vector MultiplicationBasic Math Functions

Functions

void arm_mult_f32 (float32_t *pSrcA, float32_t *pSrcB, float32_t *pDst, uint32_t blockSize)
 Floating-point vector multiplication.
 
void arm_mult_q15 (q15_t *pSrcA, q15_t *pSrcB, q15_t *pDst, uint32_t blockSize)
 Q15 vector multiplication.
 
void arm_mult_q31 (q31_t *pSrcA, q31_t *pSrcB, q31_t *pDst, uint32_t blockSize)
 Q31 vector multiplication.
 
void arm_mult_q7 (q7_t *pSrcA, q7_t *pSrcB, q7_t *pDst, uint32_t blockSize)
 Q7 vector multiplication.
 

Description

Element-by-element multiplication of two vectors.

    pDst[n] = pSrcA[n] * pSrcB[n],   0 <= n < blockSize.

There are separate functions for floating-point, Q7, Q15, and Q31 data types.

Function Documentation

void arm_mult_f32 ( float32_t pSrcA,
float32_t pSrcB,
float32_t pDst,
uint32_t  blockSize 
)
Parameters
[in]*pSrcApoints to the first input vector
[in]*pSrcBpoints to the second input vector
[out]*pDstpoints to the output vector
[in]blockSizenumber of samples in each vector
Returns
none.

References blockSize.

Referenced by arm_dct4_f32(), and main().

void arm_mult_q15 ( q15_t pSrcA,
q15_t pSrcB,
q15_t pDst,
uint32_t  blockSize 
)
Parameters
[in]*pSrcApoints to the first input vector
[in]*pSrcBpoints to the second input vector
[out]*pDstpoints to the output vector
[in]blockSizenumber of samples in each vector
Returns
none.

Scaling and Overflow Behavior:

The function uses saturating arithmetic. Results outside of the allowable Q15 range [0x8000 0x7FFF] will be saturated.

References __PKHBT, __SIMD32, and blockSize.

Referenced by arm_dct4_q15().

void arm_mult_q31 ( q31_t pSrcA,
q31_t pSrcB,
q31_t pDst,
uint32_t  blockSize 
)
Parameters
[in]*pSrcApoints to the first input vector
[in]*pSrcBpoints to the second input vector
[out]*pDstpoints to the output vector
[in]blockSizenumber of samples in each vector
Returns
none.

Scaling and Overflow Behavior:

The function uses saturating arithmetic. Results outside of the allowable Q31 range[0x80000000 0x7FFFFFFF] will be saturated.

References blockSize, and clip_q63_to_q31().

Referenced by arm_dct4_q31().

void arm_mult_q7 ( q7_t pSrcA,
q7_t pSrcB,
q7_t pDst,
uint32_t  blockSize 
)
Parameters
[in]*pSrcApoints to the first input vector
[in]*pSrcBpoints to the second input vector
[out]*pDstpoints to the output vector
[in]blockSizenumber of samples in each vector
Returns
none.

Scaling and Overflow Behavior:

The function uses saturating arithmetic. Results outside of the allowable Q7 range [0x80 0x7F] will be saturated.

References __PACKq7, __SIMD32, and blockSize.