Linear InterpolationInterpolation Functions

Functions

CMSIS_INLINE __STATIC_INLINE
float32_t 
arm_linear_interp_f32 (arm_linear_interp_instance_f32 *S, float32_t x)
 Process function for the floating-point Linear Interpolation Function.
 
CMSIS_INLINE __STATIC_INLINE q31_t arm_linear_interp_q31 (q31_t *pYData, q31_t x, uint32_t nValues)
 Process function for the Q31 Linear Interpolation Function.
 
CMSIS_INLINE __STATIC_INLINE q15_t arm_linear_interp_q15 (q15_t *pYData, q31_t x, uint32_t nValues)
 Process function for the Q15 Linear Interpolation Function.
 
CMSIS_INLINE __STATIC_INLINE q7_t arm_linear_interp_q7 (q7_t *pYData, q31_t x, uint32_t nValues)
 Process function for the Q7 Linear Interpolation Function.
 

Description

Linear interpolation is a method of curve fitting using linear polynomials. Linear interpolation works by effectively drawing a straight line between two neighboring samples and returning the appropriate point along that line

LinearInterp.gif
Linear interpolation
A Linear Interpolate function calculates an output value(y), for the input(x) using linear interpolation of the input values x0, x1( nearest input values) and the output values y0 and y1(nearest output values)
Algorithm:
      y = y0 + (x - x0) * ((y1 - y0)/(x1-x0))
      where x0, x1 are nearest values of input x
            y0, y1 are nearest values to output y
This set of functions implements Linear interpolation process for Q7, Q15, Q31, and floating-point data types. The functions operate on a single sample of data and each call to the function returns a single processed value. S points to an instance of the Linear Interpolate function data structure. x is the input sample value. The functions returns the output value.
if x is outside of the table boundary, Linear interpolation returns first value of the table if x is below input range and returns last value of table if x is above range.

Function Documentation

CMSIS_INLINE __STATIC_INLINE float32_t arm_linear_interp_f32 ( arm_linear_interp_instance_f32 S,
float32_t 
)
Parameters
[in,out]Sis an instance of the floating-point Linear Interpolation structure
[in]xinput sample to process
Returns
y processed output sample.
Examples:
arm_linear_interp_example_f32.c.

References arm_linear_interp_instance_f32::nValues, arm_linear_interp_instance_f32::pYData, arm_linear_interp_instance_f32::x1, and arm_linear_interp_instance_f32::xSpacing.

Referenced by main().

CMSIS_INLINE __STATIC_INLINE q15_t arm_linear_interp_q15 ( q15_t pYData,
q31_t  x,
uint32_t  nValues 
)
Parameters
[in]pYDatapointer to Q15 Linear Interpolation table
[in]xinput sample to process
[in]nValuesnumber of table values
Returns
y processed output sample.
Input sample x is in 12.20 format which contains 12 bits for table index and 20 bits for fractional part. This function can support maximum of table size 2^12.
CMSIS_INLINE __STATIC_INLINE q31_t arm_linear_interp_q31 ( q31_t pYData,
q31_t  x,
uint32_t  nValues 
)
Parameters
[in]pYDatapointer to Q31 Linear Interpolation table
[in]xinput sample to process
[in]nValuesnumber of table values
Returns
y processed output sample.
Input sample x is in 12.20 format which contains 12 bits for table index and 20 bits for fractional part. This function can support maximum of table size 2^12.
CMSIS_INLINE __STATIC_INLINE q7_t arm_linear_interp_q7 ( q7_t pYData,
q31_t  x,
uint32_t  nValues 
)
Parameters
[in]pYDatapointer to Q7 Linear Interpolation table
[in]xinput sample to process
[in]nValuesnumber of table values
Returns
y processed output sample.
Input sample x is in 12.20 format which contains 12 bits for table index and 20 bits for fractional part. This function can support maximum of table size 2^12.