Matrix SubtractionMatrix Functions

Functions

arm_status arm_mat_sub_f32 (const arm_matrix_instance_f32 *pSrcA, const arm_matrix_instance_f32 *pSrcB, arm_matrix_instance_f32 *pDst)
 Floating-point matrix subtraction.
 
arm_status arm_mat_sub_q15 (const arm_matrix_instance_q15 *pSrcA, const arm_matrix_instance_q15 *pSrcB, arm_matrix_instance_q15 *pDst)
 Q15 matrix subtraction.
 
arm_status arm_mat_sub_q31 (const arm_matrix_instance_q31 *pSrcA, const arm_matrix_instance_q31 *pSrcB, arm_matrix_instance_q31 *pDst)
 Q31 matrix subtraction.
 

Description

Subtract two matrices.

MatrixSubtraction.gif
Subraction of two 3 x 3 matrices

The functions check to make sure that pSrcA, pSrcB, and pDst have the same number of rows and columns.

Function Documentation

arm_status arm_mat_sub_f32 ( const arm_matrix_instance_f32 pSrcA,
const arm_matrix_instance_f32 pSrcB,
arm_matrix_instance_f32 pDst 
)
Parameters
[in]*pSrcApoints to the first input matrix structure
[in]*pSrcBpoints to the second input matrix structure
[out]*pDstpoints to output matrix structure
Returns
The function returns either ARM_MATH_SIZE_MISMATCH or ARM_MATH_SUCCESS based on the outcome of size checking.

References ARM_MATH_SIZE_MISMATCH, ARM_MATH_SUCCESS, arm_matrix_instance_f32::numCols, arm_matrix_instance_f32::numRows, arm_matrix_instance_f32::pData, and status.

arm_status arm_mat_sub_q15 ( const arm_matrix_instance_q15 pSrcA,
const arm_matrix_instance_q15 pSrcB,
arm_matrix_instance_q15 pDst 
)
Parameters
[in]*pSrcApoints to the first input matrix structure
[in]*pSrcBpoints to the second input matrix structure
[out]*pDstpoints to output matrix structure
Returns
The function returns either ARM_MATH_SIZE_MISMATCH or ARM_MATH_SUCCESS based on the outcome of size checking.

Scaling and Overflow Behavior:

The function uses saturating arithmetic. Results outside of the allowable Q15 range [0x8000 0x7FFF] will be saturated.

References __QSUB16(), __SIMD32, ARM_MATH_SIZE_MISMATCH, ARM_MATH_SUCCESS, arm_matrix_instance_q15::numCols, arm_matrix_instance_q15::numRows, arm_matrix_instance_q15::pData, and status.

arm_status arm_mat_sub_q31 ( const arm_matrix_instance_q31 pSrcA,
const arm_matrix_instance_q31 pSrcB,
arm_matrix_instance_q31 pDst 
)
Parameters
[in]*pSrcApoints to the first input matrix structure
[in]*pSrcBpoints to the second input matrix structure
[out]*pDstpoints to output matrix structure
Returns
The function returns either ARM_MATH_SIZE_MISMATCH or ARM_MATH_SUCCESS based on the outcome of size checking.

Scaling and Overflow Behavior:

The function uses saturating arithmetic. Results outside of the allowable Q31 range [0x80000000 0x7FFFFFFF] will be saturated.

References __QSUB(), ARM_MATH_SIZE_MISMATCH, ARM_MATH_SUCCESS, arm_matrix_instance_q31::numCols, arm_matrix_instance_q31::numRows, arm_matrix_instance_q31::pData, and status.