MinimumStatistics Functions

Functions

void arm_min_f32 (float32_t *pSrc, uint32_t blockSize, float32_t *pResult, uint32_t *pIndex)
 Minimum value of a floating-point vector.
 
void arm_min_q15 (q15_t *pSrc, uint32_t blockSize, q15_t *pResult, uint32_t *pIndex)
 Minimum value of a Q15 vector.
 
void arm_min_q31 (q31_t *pSrc, uint32_t blockSize, q31_t *pResult, uint32_t *pIndex)
 Minimum value of a Q31 vector.
 
void arm_min_q7 (q7_t *pSrc, uint32_t blockSize, q7_t *pResult, uint32_t *pIndex)
 Minimum value of a Q7 vector.
 

Description

Computes the minimum value of an array of data. The function returns both the minimum value and its position within the array. There are separate functions for floating-point, Q31, Q15, and Q7 data types.

Function Documentation

void arm_min_f32 ( float32_t pSrc,
uint32_t  blockSize,
float32_t pResult,
uint32_t *  pIndex 
)
Parameters
[in]*pSrcpoints to the input vector
[in]blockSizelength of the input vector
[out]*pResultminimum value returned here
[out]*pIndexindex of minimum value returned here
Returns
none.

Referenced by main().

void arm_min_q15 ( q15_t pSrc,
uint32_t  blockSize,
q15_t pResult,
uint32_t *  pIndex 
)
Parameters
[in]*pSrcpoints to the input vector
[in]blockSizelength of the input vector
[out]*pResultminimum value returned here
[out]*pIndexindex of minimum value returned here
Returns
none.
void arm_min_q31 ( q31_t pSrc,
uint32_t  blockSize,
q31_t pResult,
uint32_t *  pIndex 
)
Parameters
[in]*pSrcpoints to the input vector
[in]blockSizelength of the input vector
[out]*pResultminimum value returned here
[out]*pIndexindex of minimum value returned here
Returns
none.
void arm_min_q7 ( q7_t pSrc,
uint32_t  blockSize,
q7_t pResult,
uint32_t *  pIndex 
)
Parameters
[in]*pSrcpoints to the input vector
[in]blockSizelength of the input vector
[out]*pResultminimum value returned here
[out]*pIndexindex of minimum value returned here
Returns
none.