MeanStatistics Functions

Functions

void arm_mean_f32 (float32_t *pSrc, uint32_t blockSize, float32_t *pResult)
 Mean value of a floating-point vector.
 
void arm_mean_q15 (q15_t *pSrc, uint32_t blockSize, q15_t *pResult)
 Mean value of a Q15 vector.
 
void arm_mean_q31 (q31_t *pSrc, uint32_t blockSize, q31_t *pResult)
 Mean value of a Q31 vector.
 
void arm_mean_q7 (q7_t *pSrc, uint32_t blockSize, q7_t *pResult)
 Mean value of a Q7 vector.
 

Description

Calculates the mean of the input vector. Mean is defined as the average of the elements in the vector. The underlying algorithm is used:

        Result = (pSrc[0] + pSrc[1] + pSrc[2] + ... + pSrc[blockSize-1]) / blockSize;

There are separate functions for floating-point, Q31, Q15, and Q7 data types.

Function Documentation

void arm_mean_f32 ( float32_t pSrc,
uint32_t  blockSize,
float32_t pResult 
)
Parameters
[in]*pSrcpoints to the input vector
[in]blockSizelength of the input vector
[out]*pResultmean value returned here
Returns
none.

References blockSize.

Referenced by main().

void arm_mean_q15 ( q15_t pSrc,
uint32_t  blockSize,
q15_t pResult 
)
Parameters
[in]*pSrcpoints to the input vector
[in]blockSizelength of the input vector
[out]*pResultmean value returned here
Returns
none.

Scaling and Overflow Behavior:

The function is implemented using a 32-bit internal accumulator. The input is represented in 1.15 format and is accumulated in a 32-bit accumulator in 17.15 format. There is no risk of internal overflow with this approach, and the full precision of intermediate result is preserved. Finally, the accumulator is saturated and truncated to yield a result of 1.15 format.

References __SIMD32, and blockSize.

void arm_mean_q31 ( q31_t pSrc,
uint32_t  blockSize,
q31_t pResult 
)
Parameters
[in]*pSrcpoints to the input vector
[in]blockSizelength of the input vector
[out]*pResultmean value returned here
Returns
none.

Scaling and Overflow Behavior:

The function is implemented using a 64-bit internal accumulator. The input is represented in 1.31 format and is accumulated in a 64-bit accumulator in 33.31 format. There is no risk of internal overflow with this approach, and the full precision of intermediate result is preserved. Finally, the accumulator is truncated to yield a result of 1.31 format.

References blockSize.

void arm_mean_q7 ( q7_t pSrc,
uint32_t  blockSize,
q7_t pResult 
)
Parameters
[in]*pSrcpoints to the input vector
[in]blockSizelength of the input vector
[out]*pResultmean value returned here
Returns
none.

Scaling and Overflow Behavior:

The function is implemented using a 32-bit internal accumulator. The input is represented in 1.7 format and is accumulated in a 32-bit accumulator in 25.7 format. There is no risk of internal overflow with this approach, and the full precision of intermediate result is preserved. Finally, the accumulator is truncated to yield a result of 1.7 format.

References __SIMD32, and blockSize.