Vector NegateBasic Math Functions

Functions

void arm_negate_f32 (float32_t *pSrc, float32_t *pDst, uint32_t blockSize)
 Negates the elements of a floating-point vector.
 
void arm_negate_q15 (q15_t *pSrc, q15_t *pDst, uint32_t blockSize)
 Negates the elements of a Q15 vector.
 
void arm_negate_q31 (q31_t *pSrc, q31_t *pDst, uint32_t blockSize)
 Negates the elements of a Q31 vector.
 
void arm_negate_q7 (q7_t *pSrc, q7_t *pDst, uint32_t blockSize)
 Negates the elements of a Q7 vector.
 

Description

Negates the elements of a vector.

    pDst[n] = -pSrc[n],   0 <= n < blockSize.

The functions support in-place computation allowing the source and destination pointers to reference the same memory buffer. There are separate functions for floating-point, Q7, Q15, and Q31 data types.

Function Documentation

void arm_negate_f32 ( float32_t pSrc,
float32_t pDst,
uint32_t  blockSize 
)
Parameters
[in]*pSrcpoints to the input vector
[out]*pDstpoints to the output vector
[in]blockSizenumber of samples in the vector
Returns
none.

References blockSize.

void arm_negate_q15 ( q15_t pSrc,
q15_t pDst,
uint32_t  blockSize 
)
Parameters
[in]*pSrcpoints to the input vector
[out]*pDstpoints to the output vector
[in]blockSizenumber of samples in the vector
Returns
none.
Conditions for optimum performance
Input and output buffers should be aligned by 32-bit

Scaling and Overflow Behavior:

The function uses saturating arithmetic. The Q15 value -1 (0x8000) will be saturated to the maximum allowable positive value 0x7FFF.

References __QSUB16(), _SIMD32_OFFSET, and blockSize.

void arm_negate_q31 ( q31_t pSrc,
q31_t pDst,
uint32_t  blockSize 
)
Parameters
[in]*pSrcpoints to the input vector
[out]*pDstpoints to the output vector
[in]blockSizenumber of samples in the vector
Returns
none.

Scaling and Overflow Behavior:

The function uses saturating arithmetic. The Q31 value -1 (0x80000000) will be saturated to the maximum allowable positive value 0x7FFFFFFF.

References __QSUB(), and blockSize.

void arm_negate_q7 ( q7_t pSrc,
q7_t pDst,
uint32_t  blockSize 
)
Parameters
[in]*pSrcpoints to the input vector
[out]*pDstpoints to the output vector
[in]blockSizenumber of samples in the vector
Returns
none.

Scaling and Overflow Behavior:

The function uses saturating arithmetic. The Q7 value -1 (0x80) will be saturated to the maximum allowable positive value 0x7F.

References __QSUB8(), __SIMD32, and blockSize.