Vector FillSupport Functions
Functions | |
void | arm_fill_f32 (float32_t value, float32_t *pDst, uint32_t blockSize) |
Fills a constant value into a floating-point vector. | |
void | arm_fill_q15 (q15_t value, q15_t *pDst, uint32_t blockSize) |
Fills a constant value into a Q15 vector. | |
void | arm_fill_q31 (q31_t value, q31_t *pDst, uint32_t blockSize) |
Fills a constant value into a Q31 vector. | |
void | arm_fill_q7 (q7_t value, q7_t *pDst, uint32_t blockSize) |
Fills a constant value into a Q7 vector. | |
Description
Fills the destination vector with a constant value.
pDst[n] = value; 0 <= n < blockSize.
There are separate functions for floating point, Q31, Q15, and Q7 data types.
Function Documentation
- Parameters
-
[in] value
input value to be filled [out] *pDst
points to output vector [in] blockSize
length of the output vector
- Returns
- none.
References __PKHBT, __SIMD32, and blockSize.
Referenced by arm_conv_fast_opt_q15(), arm_conv_opt_q15(), arm_conv_opt_q7(), arm_conv_partial_fast_opt_q15(), arm_conv_partial_opt_q15(), arm_conv_partial_opt_q7(), arm_correlate_fast_opt_q15(), arm_correlate_opt_q15(), and arm_correlate_opt_q7().
- Parameters
-
[in] value
input value to be filled [out] *pDst
points to output vector [in] blockSize
length of the output vector
- Returns
- none.
References blockSize.