Infinite Impulse Response (IIR) Lattice FiltersFiltering Functions
Functions | |
void | arm_iir_lattice_f32 (const arm_iir_lattice_instance_f32 *S, float32_t *pSrc, float32_t *pDst, uint32_t blockSize) |
Processing function for the floating-point IIR lattice filter. | |
void | arm_iir_lattice_init_f32 (arm_iir_lattice_instance_f32 *S, uint16_t numStages, float32_t *pkCoeffs, float32_t *pvCoeffs, float32_t *pState, uint32_t blockSize) |
Initialization function for the floating-point IIR lattice filter. | |
void | arm_iir_lattice_init_q15 (arm_iir_lattice_instance_q15 *S, uint16_t numStages, q15_t *pkCoeffs, q15_t *pvCoeffs, q15_t *pState, uint32_t blockSize) |
Initialization function for the Q15 IIR lattice filter. | |
void | arm_iir_lattice_init_q31 (arm_iir_lattice_instance_q31 *S, uint16_t numStages, q31_t *pkCoeffs, q31_t *pvCoeffs, q31_t *pState, uint32_t blockSize) |
Initialization function for the Q31 IIR lattice filter. | |
void | arm_iir_lattice_q15 (const arm_iir_lattice_instance_q15 *S, q15_t *pSrc, q15_t *pDst, uint32_t blockSize) |
Processing function for the Q15 IIR lattice filter. | |
void | arm_iir_lattice_q31 (const arm_iir_lattice_instance_q31 *S, q31_t *pSrc, q31_t *pDst, uint32_t blockSize) |
Processing function for the Q31 IIR lattice filter. | |
Description
This set of functions implements lattice filters for Q15, Q31 and floating-point data types. Lattice filters are used in a variety of adaptive filter applications. The filter structure has feedforward and feedback components and the net impulse response is infinite length. The functions operate on blocks of input and output data and each call to the function processes blockSize
samples through the filter. pSrc
and pDst
point to input and output arrays containing blockSize
values.
- Algorithm:
- Infinite Impulse Response Lattice filter
fN(n) = x(n) fm-1(n) = fm(n) - km * gm-1(n-1) for m = N, N-1, ...1 gm(n) = km * fm-1(n) + gm-1(n-1) for m = N, N-1, ...1 y(n) = vN * gN(n) + vN-1 * gN-1(n) + ...+ v0 * g0(n)
pkCoeffs
points to array of reflection coefficients of sizenumStages
. Reflection coefficients are stored in time-reversed order.
{kN, kN-1, ....k1}
pvCoeffs
points to the array of ladder coefficients of size(numStages+1)
. Ladder coefficients are stored in time-reversed order.
{vN, vN-1, ...v0}
pState
points to a state array of sizenumStages + blockSize
. The state variables shown in the figure above (the g values) are stored in thepState
array. The state variables are updated after each block of data is processed; the coefficients are untouched.
- Instance Structure
- The coefficients and state variables for a filter are stored together in an instance data structure. A separate instance structure must be defined for each filter. Coefficient arrays may be shared among several instances while state variable arrays cannot be shared. There are separate instance structure declarations for each of the 3 supported data types.
- Initialization Functions
- There is also an associated initialization function for each data type. The initialization function performs the following operations:
- Sets the values of the internal structure fields.
- Zeros out the values in the state buffer. To do this manually without calling the init function, assign the follow subfields of the instance structure: numStages, pkCoeffs, pvCoeffs, pState. Also set all of the values in pState to zero.
- Use of the initialization function is optional. However, if the initialization function is used, then the instance structure cannot be placed into a const data section. To place an instance structure into a const data section, the instance structure must be manually initialized. Set the values in the state buffer to zeros and then manually initialize the instance structure as follows:
arm_iir_lattice_instance_f32 S = {numStages, pState, pkCoeffs, pvCoeffs}; arm_iir_lattice_instance_q31 S = {numStages, pState, pkCoeffs, pvCoeffs}; arm_iir_lattice_instance_q15 S = {numStages, pState, pkCoeffs, pvCoeffs};
- where
numStages
is the number of stages in the filter;pState
points to the state buffer array;pkCoeffs
points to array of the reflection coefficients;pvCoeffs
points to the array of ladder coefficients.
- Fixed-Point Behavior
- Care must be taken when using the fixed-point versions of the IIR lattice filter functions. In particular, the overflow and saturation behavior of the accumulator used in each function must be considered. Refer to the function specific documentation below for usage guidelines.
Function Documentation
void arm_iir_lattice_f32 | ( | const arm_iir_lattice_instance_f32 * | S, |
float32_t * | pSrc, |
||
float32_t * | pDst, |
||
uint32_t | blockSize |
||
) |
- Parameters
-
[in] *S
points to an instance of the floating-point IIR lattice structure. [in] *pSrc
points to the block of input data. [out] *pDst
points to the block of output data. [in] blockSize
number of samples to process.
- Returns
- none.
References blockSize, arm_iir_lattice_instance_f32::numStages, arm_iir_lattice_instance_f32::pkCoeffs, arm_iir_lattice_instance_f32::pState, and arm_iir_lattice_instance_f32::pvCoeffs.
void arm_iir_lattice_init_f32 | ( | arm_iir_lattice_instance_f32 * | S, |
uint16_t | numStages, |
||
float32_t * | pkCoeffs, |
||
float32_t * | pvCoeffs, |
||
float32_t * | pState, |
||
uint32_t | blockSize |
||
) |
- Parameters
-
[in] *S
points to an instance of the floating-point IIR lattice structure. [in] numStages
number of stages in the filter. [in] *pkCoeffs
points to the reflection coefficient buffer. The array is of length numStages. [in] *pvCoeffs
points to the ladder coefficient buffer. The array is of length numStages+1. [in] *pState
points to the state buffer. The array is of length numStages+blockSize. [in] blockSize
number of samples to process.
- Returns
- none.
References arm_iir_lattice_instance_f32::numStages, arm_iir_lattice_instance_f32::pkCoeffs, arm_iir_lattice_instance_f32::pState, and arm_iir_lattice_instance_f32::pvCoeffs.
void arm_iir_lattice_init_q15 | ( | arm_iir_lattice_instance_q15 * | S, |
uint16_t | numStages, |
||
q15_t * | pkCoeffs, |
||
q15_t * | pvCoeffs, |
||
q15_t * | pState, |
||
uint32_t | blockSize |
||
) |
- Parameters
-
[in] *S
points to an instance of the Q15 IIR lattice structure. [in] numStages
number of stages in the filter. [in] *pkCoeffs
points to reflection coefficient buffer. The array is of length numStages. [in] *pvCoeffs
points to ladder coefficient buffer. The array is of length numStages+1. [in] *pState
points to state buffer. The array is of length numStages+blockSize. [in] blockSize
number of samples to process per call.
- Returns
- none.
References arm_iir_lattice_instance_q15::numStages, arm_iir_lattice_instance_q15::pkCoeffs, arm_iir_lattice_instance_q15::pState, and arm_iir_lattice_instance_q15::pvCoeffs.
void arm_iir_lattice_init_q31 | ( | arm_iir_lattice_instance_q31 * | S, |
uint16_t | numStages, |
||
q31_t * | pkCoeffs, |
||
q31_t * | pvCoeffs, |
||
q31_t * | pState, |
||
uint32_t | blockSize |
||
) |
- Parameters
-
[in] *S
points to an instance of the Q31 IIR lattice structure. [in] numStages
number of stages in the filter. [in] *pkCoeffs
points to the reflection coefficient buffer. The array is of length numStages. [in] *pvCoeffs
points to the ladder coefficient buffer. The array is of length numStages+1. [in] *pState
points to the state buffer. The array is of length numStages+blockSize. [in] blockSize
number of samples to process.
- Returns
- none.
References arm_iir_lattice_instance_q31::numStages, arm_iir_lattice_instance_q31::pkCoeffs, arm_iir_lattice_instance_q31::pState, and arm_iir_lattice_instance_q31::pvCoeffs.
void arm_iir_lattice_q15 | ( | const arm_iir_lattice_instance_q15 * | S, |
q15_t * | pSrc, |
||
q15_t * | pDst, |
||
uint32_t | blockSize |
||
) |
- Parameters
-
[in] *S
points to an instance of the Q15 IIR lattice structure. [in] *pSrc
points to the block of input data. [out] *pDst
points to the block of output data. [in] blockSize
number of samples to process.
- Returns
- none.
Scaling and Overflow Behavior:
- The function is implemented using a 64-bit internal accumulator. Both coefficients and state variables are represented in 1.15 format and multiplications yield a 2.30 result. The 2.30 intermediate results are accumulated in a 64-bit accumulator in 34.30 format. There is no risk of internal overflow with this approach and the full precision of intermediate multiplications is preserved. After all additions have been performed, the accumulator is truncated to 34.15 format by discarding low 15 bits. Lastly, the accumulator is saturated to yield a result in 1.15 format.
References __PKHBT, __SIMD32, __SMLALD(), blockSize, arm_iir_lattice_instance_q15::numStages, arm_iir_lattice_instance_q15::pkCoeffs, arm_iir_lattice_instance_q15::pState, and arm_iir_lattice_instance_q15::pvCoeffs.
void arm_iir_lattice_q31 | ( | const arm_iir_lattice_instance_q31 * | S, |
q31_t * | pSrc, |
||
q31_t * | pDst, |
||
uint32_t | blockSize |
||
) |
- Parameters
-
[in] *S
points to an instance of the Q31 IIR lattice structure. [in] *pSrc
points to the block of input data. [out] *pDst
points to the block of output data. [in] blockSize
number of samples to process.
- Returns
- none.
Scaling and Overflow Behavior:
- The function is implemented using an internal 64-bit accumulator. The accumulator has a 2.62 format and maintains full precision of the intermediate multiplication results but provides only a single guard bit. Thus, if the accumulator result overflows it wraps around rather than clip. In order to avoid overflows completely the input signal must be scaled down by 2*log2(numStages) bits. After all multiply-accumulates are performed, the 2.62 accumulator is saturated to 1.32 format and then truncated to 1.31 format.
References __QADD(), __QSUB(), blockSize, clip_q63_to_q31(), arm_iir_lattice_instance_q31::numStages, arm_iir_lattice_instance_q31::pkCoeffs, arm_iir_lattice_instance_q31::pState, and arm_iir_lattice_instance_q31::pvCoeffs.