Matrix SubtractionMatrix Functions
Functions | |
arm_status | arm_mat_sub_f32 (const arm_matrix_instance_f32 *pSrcA, const arm_matrix_instance_f32 *pSrcB, arm_matrix_instance_f32 *pDst) |
Floating-point matrix subtraction. | |
arm_status | arm_mat_sub_q15 (const arm_matrix_instance_q15 *pSrcA, const arm_matrix_instance_q15 *pSrcB, arm_matrix_instance_q15 *pDst) |
Q15 matrix subtraction. | |
arm_status | arm_mat_sub_q31 (const arm_matrix_instance_q31 *pSrcA, const arm_matrix_instance_q31 *pSrcB, arm_matrix_instance_q31 *pDst) |
Q31 matrix subtraction. | |
Description
Subtract two matrices.

Subraction of two 3 x 3 matrices
The functions check to make sure that pSrcA
, pSrcB
, and pDst
have the same number of rows and columns.
Function Documentation
arm_status arm_mat_sub_f32 | ( | const arm_matrix_instance_f32 * | pSrcA, |
const arm_matrix_instance_f32 * | pSrcB, |
||
arm_matrix_instance_f32 * | pDst |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input matrix structure [in] *pSrcB
points to the second input matrix structure [out] *pDst
points to output matrix structure
- Returns
- The function returns either
ARM_MATH_SIZE_MISMATCH
orARM_MATH_SUCCESS
based on the outcome of size checking.
References ARM_MATH_SIZE_MISMATCH, ARM_MATH_SUCCESS, arm_matrix_instance_f32::numCols, arm_matrix_instance_f32::numRows, arm_matrix_instance_f32::pData, and status.
arm_status arm_mat_sub_q15 | ( | const arm_matrix_instance_q15 * | pSrcA, |
const arm_matrix_instance_q15 * | pSrcB, |
||
arm_matrix_instance_q15 * | pDst |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input matrix structure [in] *pSrcB
points to the second input matrix structure [out] *pDst
points to output matrix structure
- Returns
- The function returns either
ARM_MATH_SIZE_MISMATCH
orARM_MATH_SUCCESS
based on the outcome of size checking.
Scaling and Overflow Behavior:
- The function uses saturating arithmetic. Results outside of the allowable Q15 range [0x8000 0x7FFF] will be saturated.
References __QSUB16(), __SIMD32, ARM_MATH_SIZE_MISMATCH, ARM_MATH_SUCCESS, arm_matrix_instance_q15::numCols, arm_matrix_instance_q15::numRows, arm_matrix_instance_q15::pData, and status.
arm_status arm_mat_sub_q31 | ( | const arm_matrix_instance_q31 * | pSrcA, |
const arm_matrix_instance_q31 * | pSrcB, |
||
arm_matrix_instance_q31 * | pDst |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input matrix structure [in] *pSrcB
points to the second input matrix structure [out] *pDst
points to output matrix structure
- Returns
- The function returns either
ARM_MATH_SIZE_MISMATCH
orARM_MATH_SUCCESS
based on the outcome of size checking.
Scaling and Overflow Behavior:
- The function uses saturating arithmetic. Results outside of the allowable Q31 range [0x80000000 0x7FFFFFFF] will be saturated.
References __QSUB(), ARM_MATH_SIZE_MISMATCH, ARM_MATH_SUCCESS, arm_matrix_instance_q31::numCols, arm_matrix_instance_q31::numRows, arm_matrix_instance_q31::pData, and status.