MinimumStatistics Functions
Functions | |
void | arm_min_f32 (float32_t *pSrc, uint32_t blockSize, float32_t *pResult, uint32_t *pIndex) |
Minimum value of a floating-point vector. | |
void | arm_min_q15 (q15_t *pSrc, uint32_t blockSize, q15_t *pResult, uint32_t *pIndex) |
Minimum value of a Q15 vector. | |
void | arm_min_q31 (q31_t *pSrc, uint32_t blockSize, q31_t *pResult, uint32_t *pIndex) |
Minimum value of a Q31 vector. | |
void | arm_min_q7 (q7_t *pSrc, uint32_t blockSize, q7_t *pResult, uint32_t *pIndex) |
Minimum value of a Q7 vector. | |
Description
Computes the minimum value of an array of data. The function returns both the minimum value and its position within the array. There are separate functions for floating-point, Q31, Q15, and Q7 data types.
Function Documentation
- Parameters
-
[in] *pSrc
points to the input vector [in] blockSize
length of the input vector [out] *pResult
minimum value returned here [out] *pIndex
index of minimum value returned here
- Returns
- none.
Referenced by main().
- Parameters
-
[in] *pSrc
points to the input vector [in] blockSize
length of the input vector [out] *pResult
minimum value returned here [out] *pIndex
index of minimum value returned here
- Returns
- none.
- Parameters
-
[in] *pSrc
points to the input vector [in] blockSize
length of the input vector [out] *pResult
minimum value returned here [out] *pIndex
index of minimum value returned here
- Returns
- none.