Partial ConvolutionFiltering Functions
Functions | |
arm_status | arm_conv_partial_f32 (float32_t *pSrcA, uint32_t srcALen, float32_t *pSrcB, uint32_t srcBLen, float32_t *pDst, uint32_t firstIndex, uint32_t numPoints) |
Partial convolution of floating-point sequences. | |
arm_status | arm_conv_partial_fast_opt_q15 (q15_t *pSrcA, uint32_t srcALen, q15_t *pSrcB, uint32_t srcBLen, q15_t *pDst, uint32_t firstIndex, uint32_t numPoints, q15_t *pScratch1, q15_t *pScratch2) |
Partial convolution of Q15 sequences (fast version) for Cortex-M3 and Cortex-M4. | |
arm_status | arm_conv_partial_fast_q15 (q15_t *pSrcA, uint32_t srcALen, q15_t *pSrcB, uint32_t srcBLen, q15_t *pDst, uint32_t firstIndex, uint32_t numPoints) |
Partial convolution of Q15 sequences (fast version) for Cortex-M3 and Cortex-M4. | |
arm_status | arm_conv_partial_fast_q31 (q31_t *pSrcA, uint32_t srcALen, q31_t *pSrcB, uint32_t srcBLen, q31_t *pDst, uint32_t firstIndex, uint32_t numPoints) |
Partial convolution of Q31 sequences (fast version) for Cortex-M3 and Cortex-M4. | |
arm_status | arm_conv_partial_opt_q15 (q15_t *pSrcA, uint32_t srcALen, q15_t *pSrcB, uint32_t srcBLen, q15_t *pDst, uint32_t firstIndex, uint32_t numPoints, q15_t *pScratch1, q15_t *pScratch2) |
Partial convolution of Q15 sequences. | |
arm_status | arm_conv_partial_opt_q7 (q7_t *pSrcA, uint32_t srcALen, q7_t *pSrcB, uint32_t srcBLen, q7_t *pDst, uint32_t firstIndex, uint32_t numPoints, q15_t *pScratch1, q15_t *pScratch2) |
Partial convolution of Q7 sequences. | |
arm_status | arm_conv_partial_q15 (q15_t *pSrcA, uint32_t srcALen, q15_t *pSrcB, uint32_t srcBLen, q15_t *pDst, uint32_t firstIndex, uint32_t numPoints) |
Partial convolution of Q15 sequences. | |
arm_status | arm_conv_partial_q31 (q31_t *pSrcA, uint32_t srcALen, q31_t *pSrcB, uint32_t srcBLen, q31_t *pDst, uint32_t firstIndex, uint32_t numPoints) |
Partial convolution of Q31 sequences. | |
arm_status | arm_conv_partial_q7 (q7_t *pSrcA, uint32_t srcALen, q7_t *pSrcB, uint32_t srcBLen, q7_t *pDst, uint32_t firstIndex, uint32_t numPoints) |
Partial convolution of Q7 sequences. | |
Description
Partial Convolution is equivalent to Convolution except that a subset of the output samples is generated. Each function has two additional arguments. firstIndex
specifies the starting index of the subset of output samples. numPoints
is the number of output samples to compute. The function computes the output in the range [firstIndex, ..., firstIndex+numPoints-1]
. The output array pDst
contains numPoints
values.
The allowable range of output indices is [0 srcALen+srcBLen-2]. If the requested subset does not fall in this range then the functions return ARM_MATH_ARGUMENT_ERROR. Otherwise the functions return ARM_MATH_SUCCESS.
- Note
- Refer arm_conv_f32() for details on fixed point behavior.
Fast Versions
- Fast versions are supported for Q31 and Q15 of partial convolution. Cycles for Fast versions are less compared to Q31 and Q15 of partial conv and the design requires the input signals should be scaled down to avoid intermediate overflows.
Opt Versions
- Opt versions are supported for Q15 and Q7. Design uses internal scratch buffer for getting good optimisation. These versions are optimised in cycles and consumes more memory(Scratch memory) compared to Q15 and Q7 versions of partial convolution
Function Documentation
arm_status arm_conv_partial_f32 | ( | float32_t * | pSrcA, |
uint32_t | srcALen, |
||
float32_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
float32_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed.
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
References ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.
arm_status arm_conv_partial_fast_opt_q15 | ( | q15_t * | pSrcA, |
uint32_t | srcALen, |
||
q15_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
q15_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints, |
||
q15_t * | pScratch1, |
||
q15_t * | pScratch2 |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed. [in] *pScratch1
points to scratch buffer of size max(srcALen, srcBLen) + 2*min(srcALen, srcBLen) - 2. [in] *pScratch2
points to scratch buffer of size min(srcALen, srcBLen).
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
See arm_conv_partial_q15()
for a slower implementation of this function which uses a 64-bit accumulator to avoid wrap around distortion.
- Restrictions
- If the silicon does not support unaligned memory access enable the macro UNALIGNED_SUPPORT_DISABLE In this case input, output, scratch1 and scratch2 buffers should be aligned by 32-bit
References __PKHBT, __SIMD32, __SMLAD(), __SMLADX(), _SIMD32_OFFSET, arm_copy_q15(), arm_fill_q15(), ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.
arm_status arm_conv_partial_fast_q15 | ( | q15_t * | pSrcA, |
uint32_t | srcALen, |
||
q15_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
q15_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed.
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
See arm_conv_partial_q15()
for a slower implementation of this function which uses a 64-bit accumulator to avoid wrap around distortion.
References __PKHBT, __SIMD32, __SMLAD(), __SMLADX(), _SIMD32_OFFSET, ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.
arm_status arm_conv_partial_fast_q31 | ( | q31_t * | pSrcA, |
uint32_t | srcALen, |
||
q31_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
q31_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed.
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
- See
arm_conv_partial_q31()
for a slower implementation of this function which uses a 64-bit accumulator to provide higher precision.
References ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.
arm_status arm_conv_partial_opt_q15 | ( | q15_t * | pSrcA, |
uint32_t | srcALen, |
||
q15_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
q15_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints, |
||
q15_t * | pScratch1, |
||
q15_t * | pScratch2 |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed. [in] *pScratch1
points to scratch buffer of size max(srcALen, srcBLen) + 2*min(srcALen, srcBLen) - 2. [in] *pScratch2
points to scratch buffer of size min(srcALen, srcBLen).
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
- Restrictions
- If the silicon does not support unaligned memory access enable the macro UNALIGNED_SUPPORT_DISABLE In this case input, output, state buffers should be aligned by 32-bit
Refer to arm_conv_partial_fast_q15()
for a faster but less precise version of this function for Cortex-M3 and Cortex-M4.
References __PKHBT, __SIMD32, __SMLALD(), __SMLALDX(), _SIMD32_OFFSET, arm_copy_q15(), arm_fill_q15(), ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.
arm_status arm_conv_partial_opt_q7 | ( | q7_t * | pSrcA, |
uint32_t | srcALen, |
||
q7_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
q7_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints, |
||
q15_t * | pScratch1, |
||
q15_t * | pScratch2 |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed. [in] *pScratch1
points to scratch buffer(of type q15_t) of size max(srcALen, srcBLen) + 2*min(srcALen, srcBLen) - 2. [in] *pScratch2
points to scratch buffer (of type q15_t) of size min(srcALen, srcBLen).
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
- Restrictions
- If the silicon does not support unaligned memory access enable the macro UNALIGNED_SUPPORT_DISABLE In this case input, output, scratch1 and scratch2 buffers should be aligned by 32-bit
References __PACKq7, __PKHBT, __SIMD32, __SMLAD(), __SMLADX(), _SIMD32_OFFSET, arm_fill_q15(), ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.
arm_status arm_conv_partial_q15 | ( | q15_t * | pSrcA, |
uint32_t | srcALen, |
||
q15_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
q15_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed.
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
Refer to arm_conv_partial_fast_q15()
for a faster but less precise version of this function for Cortex-M3 and Cortex-M4.
- Refer the function
arm_conv_partial_opt_q15()
for a faster implementation of this function using scratch buffers.
References __PKHBT, __SIMD32, __SMLALD(), __SMLALDX(), _SIMD32_OFFSET, ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.
arm_status arm_conv_partial_q31 | ( | q31_t * | pSrcA, |
uint32_t | srcALen, |
||
q31_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
q31_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed.
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
See arm_conv_partial_fast_q31()
for a faster but less precise implementation of this function for Cortex-M3 and Cortex-M4.
References ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.
arm_status arm_conv_partial_q7 | ( | q7_t * | pSrcA, |
uint32_t | srcALen, |
||
q7_t * | pSrcB, |
||
uint32_t | srcBLen, |
||
q7_t * | pDst, |
||
uint32_t | firstIndex, |
||
uint32_t | numPoints |
||
) |
- Parameters
-
[in] *pSrcA
points to the first input sequence. [in] srcALen
length of the first input sequence. [in] *pSrcB
points to the second input sequence. [in] srcBLen
length of the second input sequence. [out] *pDst
points to the location where the output result is written. [in] firstIndex
is the first output sample to start with. [in] numPoints
is the number of output points to be computed.
- Returns
- Returns either ARM_MATH_SUCCESS if the function completed correctly or ARM_MATH_ARGUMENT_ERROR if the requested subset is not in the range [0 srcALen+srcBLen-2].
- Refer the function
arm_conv_partial_opt_q7()
for a faster implementation of this function.
References __SMLAD(), ARM_MATH_ARGUMENT_ERROR, ARM_MATH_SUCCESS, srcALen, srcBLen, and status.