Vector NegateBasic Math Functions
Functions | |
void | arm_negate_f32 (float32_t *pSrc, float32_t *pDst, uint32_t blockSize) |
Negates the elements of a floating-point vector. | |
void | arm_negate_q15 (q15_t *pSrc, q15_t *pDst, uint32_t blockSize) |
Negates the elements of a Q15 vector. | |
void | arm_negate_q31 (q31_t *pSrc, q31_t *pDst, uint32_t blockSize) |
Negates the elements of a Q31 vector. | |
void | arm_negate_q7 (q7_t *pSrc, q7_t *pDst, uint32_t blockSize) |
Negates the elements of a Q7 vector. | |
Description
Negates the elements of a vector.
pDst[n] = -pSrc[n], 0 <= n < blockSize.
The functions support in-place computation allowing the source and destination pointers to reference the same memory buffer. There are separate functions for floating-point, Q7, Q15, and Q31 data types.
Function Documentation
- Parameters
-
[in] *pSrc
points to the input vector [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
References blockSize.
- Parameters
-
[in] *pSrc
points to the input vector [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
- Conditions for optimum performance
- Input and output buffers should be aligned by 32-bit
Scaling and Overflow Behavior:
- The function uses saturating arithmetic. The Q15 value -1 (0x8000) will be saturated to the maximum allowable positive value 0x7FFF.
References __QSUB16(), _SIMD32_OFFSET, and blockSize.
- Parameters
-
[in] *pSrc
points to the input vector [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
Scaling and Overflow Behavior:
- The function uses saturating arithmetic. The Q31 value -1 (0x80000000) will be saturated to the maximum allowable positive value 0x7FFFFFFF.
- Parameters
-
[in] *pSrc
points to the input vector [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
Scaling and Overflow Behavior:
- The function uses saturating arithmetic. The Q7 value -1 (0x80) will be saturated to the maximum allowable positive value 0x7F.