Vector OffsetBasic Math Functions
Functions | |
void | arm_offset_f32 (float32_t *pSrc, float32_t offset, float32_t *pDst, uint32_t blockSize) |
Adds a constant offset to a floating-point vector. | |
void | arm_offset_q15 (q15_t *pSrc, q15_t offset, q15_t *pDst, uint32_t blockSize) |
Adds a constant offset to a Q15 vector. | |
void | arm_offset_q31 (q31_t *pSrc, q31_t offset, q31_t *pDst, uint32_t blockSize) |
Adds a constant offset to a Q31 vector. | |
void | arm_offset_q7 (q7_t *pSrc, q7_t offset, q7_t *pDst, uint32_t blockSize) |
Adds a constant offset to a Q7 vector. | |
Description
Adds a constant offset to each element of a vector.
pDst[n] = pSrc[n] + offset, 0 <= n < blockSize.
The functions support in-place computation allowing the source and destination pointers to reference the same memory buffer. There are separate functions for floating-point, Q7, Q15, and Q31 data types.
Function Documentation
- Parameters
-
[in] *pSrc
points to the input vector [in] offset
is the offset to be added [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
References blockSize.
- Parameters
-
[in] *pSrc
points to the input vector [in] offset
is the offset to be added [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
Scaling and Overflow Behavior:
- The function uses saturating arithmetic. Results outside of the allowable Q15 range [0x8000 0x7FFF] are saturated.
References __PKHBT, __QADD16(), __SIMD32, and blockSize.
- Parameters
-
[in] *pSrc
points to the input vector [in] offset
is the offset to be added [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
Scaling and Overflow Behavior:
- The function uses saturating arithmetic. Results outside of the allowable Q31 range [0x80000000 0x7FFFFFFF] are saturated.
References __QADD(), blockSize, and clip_q63_to_q31().
- Parameters
-
[in] *pSrc
points to the input vector [in] offset
is the offset to be added [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
Scaling and Overflow Behavior:
- The function uses saturating arithmetic. Results outside of the allowable Q7 range [0x80 0x7F] are saturated.