Vector ScaleBasic Math Functions
Functions | |
void | arm_scale_f32 (float32_t *pSrc, float32_t scale, float32_t *pDst, uint32_t blockSize) |
Multiplies a floating-point vector by a scalar. | |
void | arm_scale_q15 (q15_t *pSrc, q15_t scaleFract, int8_t shift, q15_t *pDst, uint32_t blockSize) |
Multiplies a Q15 vector by a scalar. | |
void | arm_scale_q31 (q31_t *pSrc, q31_t scaleFract, int8_t shift, q31_t *pDst, uint32_t blockSize) |
Multiplies a Q31 vector by a scalar. | |
void | arm_scale_q7 (q7_t *pSrc, q7_t scaleFract, int8_t shift, q7_t *pDst, uint32_t blockSize) |
Multiplies a Q7 vector by a scalar. | |
Description
Multiply a vector by a scalar value. For floating-point data, the algorithm used is:
pDst[n] = pSrc[n] * scale, 0 <= n < blockSize.
In the fixed-point Q7, Q15, and Q31 functions, scale
is represented by a fractional multiplication scaleFract
and an arithmetic shift shift
. The shift allows the gain of the scaling operation to exceed 1.0. The algorithm used with fixed-point data is:
pDst[n] = (pSrc[n] * scaleFract) << shift, 0 <= n < blockSize.
The overall scale factor applied to the fixed-point data is
scale = scaleFract * 2^shift.
The functions support in-place computation allowing the source and destination pointers to reference the same memory buffer.
Function Documentation
- Parameters
-
[in] *pSrc
points to the input vector [in] scale
scale factor to be applied [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
References blockSize.
Referenced by arm_dct4_f32(), and main().
void arm_scale_q15 | ( | q15_t * | pSrc, |
q15_t | scaleFract, |
||
int8_t | shift, |
||
q15_t * | pDst, |
||
uint32_t | blockSize |
||
) |
- Parameters
-
[in] *pSrc
points to the input vector [in] scaleFract
fractional portion of the scale value [in] shift
number of bits to shift the result by [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
Scaling and Overflow Behavior:
- The input data
*pSrc
andscaleFract
are in 1.15 format. These are multiplied to yield a 2.30 intermediate result and this is shifted with saturation to 1.15 format.
void arm_scale_q31 | ( | q31_t * | pSrc, |
q31_t | scaleFract, |
||
int8_t | shift, |
||
q31_t * | pDst, |
||
uint32_t | blockSize |
||
) |
- Parameters
-
[in] *pSrc
points to the input vector [in] scaleFract
fractional portion of the scale value [in] shift
number of bits to shift the result by [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
Scaling and Overflow Behavior:
- The input data
*pSrc
andscaleFract
are in 1.31 format. These are multiplied to yield a 2.62 intermediate result and this is shifted with saturation to 1.31 format.
References blockSize.
Referenced by main().
- Parameters
-
[in] *pSrc
points to the input vector [in] scaleFract
fractional portion of the scale value [in] shift
number of bits to shift the result by [out] *pDst
points to the output vector [in] blockSize
number of samples in the vector
- Returns
- none.
Scaling and Overflow Behavior:
- The input data
*pSrc
andscaleFract
are in 1.7 format. These are multiplied to yield a 2.14 intermediate result and this is shifted with saturation to 1.7 format.