/package/conditions element

The grouping element /package/conditions contains all conditions defined for the Software Pack.

A condition describes dependencies on device, processor, and tool attributes as well as the presence of other components. The conditions are used to define AND and OR rules used to make components conditional and therefore only available under certain circumstances, e.g. for specific devices or processors. The conditions are also used to express dependencies between components.

Each condition has an id that is unique within the scope of a the description. An id can be referenced in the condition attribute of components, apis, examples, files and other conditions to become conditional. If a condition resolves to false during the processing of the description, the respective element will be ignored.

Example:

<conditions>
<condition id="CM4"> <!-- defines the condition with the ID "CM4" -->
<description>True if the active device has a Cortex-M4 processor</description>
<require Dcore="Cortex-M4"/> <!-- device has a Cortex-M4 processor -->
</condition>
<condition id="Cortex-M"> <!-- defines the condition with the ID "Cortex-M" -->
<description>True if the active device has a Cortex-M0 or Cortex-M0+ or Cortex-M3 or Cortex-M4 or SC000 or SC3000 processor </description>
<accept Dcore="Cortex-M0"/> <!-- any of the following cores will make the condition resolve to true -->
<accept Dcore="Cortex-M0+"/>
<accept Dcore="Cortex-M23"/>
<accept Dcore="Cortex-M3"/>
<accept Dcore="Cortex-M33"/>
<accept Dcore="Cortex-M4"/>
<accept Dcore="SC000"/>
<accept Dcore="SC300"/>
</condition>
<condition id="CMSIS-Core"> <!-- defines the condition with the ID "CMSIS-Core" -->
<description>True if the component Device Startup is selected and the device has a Cortex-M processor</description>
<require Cclass="Device" Cgroup="Startup"/> <!-- needs a software component Device Startup AND ... -->
<require condition="Cortex-M"/> <!-- ... needs that condition with ID=Cortex-M to be true. -->
</condition>
<condition id="CMSIS-DSP"> <!-- defines the condition with the ID "CMSIS-DSP" -->
<description>True if CMSIS-Core == TRUE and either GCC or ARMCC and device running in little-endian byte ordering</description>
<require condition="CMSIS-Core"/> <!-- needs a software component Device Startup AND ... -->
<accept Tcompiler="GCC"/> <!-- ... works either with the GCC compiler OR ... -->
<accept Tcompiler="ARMCC"/> <!-- ... the ARMCC compiler AND ... -->
<require Dendian="Little-endian"/> <!-- ... requires a device running in little-endian byte ordering -->
</condition>
<condition id="No STM32"> <!-- defines the condition with ID "No STM32" -->
<description>False if the device is from ST and the device name starts with "STM32"</description>
<deny Dvendor="STMicroelectronics:13" Dname="STM32*"/> <!-- device name must not start with STM32 and be from vendor ST-->
</condition>
</conditions>

 


/package/conditions

This element groups all conditions used in the Software Pack.

Parent Chain
package /package
Child Elements Description Type Occurrence
condition Define the individual dependency condition. xs:string 1..*

 


/package/conditions/condition

Conditions are dependency rules that can apply to elements such as a component or file. Other elements can refer to a rule using their attribute condition, which links to the attribute id of a condition. If a condition resolves to false, then the component or file description is ignored.

Parent Chain
conditions /package/conditions
Attributes Description Type Use
id Condition identifier which is unique within a Software Pack. The condition identifier is referenced by other elements with the attribute condition. xs:string required
Child Elements Description Type Occurrence
description Descriptive (comment) text that explains the condition in an human readable way. xs:string 0..1
accept1 At least one accept must be true to signal a true for the complete condition (OR-Rule) FilterType 0..*
require1 All require must be true to signal a true for the complete condition (AND-Rule). FilterType 0..*
deny1 If one deny is true the complete condition becomes false. This element overrules require and accept (AND-NOT-Rule). FilterType 0..*
Note
1: At least one of these elements must be present in any condition.

 


/package/conditions/condition/accept

/package/conditions/condition/require

/package/conditions/condition/deny

All attributes set in an accept, require, or deny must resolve to true for the element to become true. A condition becomes true when:

  • At least one accept element is true, AND
  • all require elements are true, AND
  • no deny element is true.
Parent Chain
accept /package/conditions/condition/accept
require /package/conditions/condition/require
deny /package/conditions/condition/deny
Attributes Description Type Use
Dfamily* Specifies the device family name (for example: STM32F2 Series). xs:string optional
DsubFamily* Specifies the device sub-family name (for example: STM32F205 Series). xs:string optional
Dvariant* Specifies the variant name of a device (for example: Step A). xs:string optional
Dvendor Specifies the silicon vendor of the device. Use predefined values as listed in the table Device Vendor. DeviceVendorEnum optional
Dname* Specifies the name of the device. xs:string optional
Pname Specifies the processor instance in case of multi processor devices. This allows to describe distinct conditions for a specific processor. xs:string optional
Dcore Specifies a processor core. Use predefined values as listed in the table Device Cores. DcoreEnum optional
Dfpu Specifies whether a Floating Point Unit (FPU) must be present or not. Predefined values can be used as listed in the table Device FPU. DfpuEnum optional
Dmpu Specifies whether a Memory Protection Unit (MPU) must be present or not. Predefined values can be used as listed in the table Device MPU. DmpuEnum optional
Dtz Specifies whether TrustZone (TZ) must be supported by the device or not. Predefined values can be used as listed in the table Device TrustZone. DtzEnum optional
Dsecure Specifies whether Digital Signal Processing (DSP) instruction set must be supported by the device or not. Predefined values can be uses as listed in the table Device DSP. DsecureEnum optional
Ddsp Specifies whether Digital Signal Processing (DSP) instruction set must be supported by the device or not. Predefined values can be uses as listed in the table Device DSP. DdspEnum optional
Dendian Specifies the endianess of a device. Use predefined values as listed in the table Endianess. DendianEnum optional
Cvendor* Specifies a component vendor name. xs:string optional
Cbundle* Specifies a component class bundle name. xs:string optional
Cclass* Specifies a component class name. Predefined values can be used as listed in the table Component Classes. CclassType optional
Cgroup* Specifies a software Component Group. Predefined values can be used as listed in the table Component Groups. CgroupType optional
Csub* Specifies a software component subgroup. The type is described in Component Subgroups. CsubType optional
Cvariant* Specifies a software component variant. xs:string optional
Cversion Specifies a software component version.
  • require Cversion:condition is true if version of component is equal or higher than requested.
  • deny Cversion: condition is true if version of component is lower than requested.
  • Version ranges are specified with min_version:max_version. The condition is true if the version of the component is equal or higher than min_version and lower or equal than max_version. If min_version and max_version are equal the version must match. For more information refer to Version Type.
VersionType optional
Capiversion Specifies an API version.
  • require Capiversion:condition is true if version of API is equal or higher than requested.
  • deny Capiversion: condition is true if version of API is lower than requested.
  • Version ranges are specified with min_version:max_version. The condition is true if the version of the API is equal or higher than min_version and lower or equal than max_version. If min_version and max_version are equal the version must match. For more information refer to Version Type.
VersionType optional
Tcompiler Specifies a compiler toolchain (ARMCC, GCC, IAR, Tasking, ...). Use predefined values as listed in table Compiler Types. CompilerEnumType optional
Toptions

Specifies compiler specific options being active. For Tcompiler="ARMCC" available Toptions are:

  • AC5: Arm Compiler Version 5 is in used
  • AC6: Arm Compiler Version 6 (armclang) is in use
  • AC6LTO: Arm Compiler Version 6 with Link Time Optimization (LTO) is in use

This attribute can be used to select compatible libraries for the selected compiler version or optimization mode.

CompilerEnumType optional
condition Refers to another condition identified through the attribute id. xs:string optional

*) Wild-cards can be used to match names with the following definitions:

  • '*' matches any substring
  • '?' matches any single character
  • [abc] matches any character in the set (a,b,c)

 

Table: Compiler Types

The tale list values representing a C/C++ compiler toolchains from a specific tool vendor. The tokens can be used in the elements:

Tcompiler= Description
GCC GNU Tools for Arm Embedded Processors. Refer to Arm GCC.
G++ Code Sourcery GCC compiler for C and C++ (is now Mentor Graphics CodeBench).
ARMCC Arm Compiler for C and C++. Refer to Arm Compiler.
IAR IAR compiler for C and C++.
Tasking TASKING compiler for C and C++.
GHS Green Hills Software compiler for C, C++, and EC++.