License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
This notice may not be removed or altered from any source distribution.
/***************************************************************************/
void emberAfPluginPollSetShortPollInterval(uint8_t intervalQS);
void emberAfPluginPollSetLongPollInterval(uint16_t intervalS);
void emberAfPluginPollEnableShortPolling(bool enable);
Functions#
Set the short poll interval.
Set the long poll interval.
Enable/disable short polling.
Function Documentation#
emberAfPluginPollSetShortPollInterval#
void emberAfPluginPollSetShortPollInterval (uint8_t intervalQS)
Set the short poll interval.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [in] | intervalQS | The short poll interval in quarter seconds. |
emberAfPluginPollSetLongPollInterval#
void emberAfPluginPollSetLongPollInterval (uint16_t intervalS)
Set the long poll interval.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint16_t | [in] | intervalS | The long poll interval in seconds. |
emberAfPluginPollEnableShortPolling#
void emberAfPluginPollEnableShortPolling (bool enable)
Enable/disable short polling.
Type | Direction | Argument Name | Description |
---|---|---|---|
bool | [in] | enable | If this parameter is true, short polling is enabled. Otherwise, the node switches back to long polling. |