License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required. 
- Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software. 
- This notice may not be removed or altered from any source distribution. 
/***************************************************************************/
#ifndef SILABS_ERROR_DEF_H
#define SILABS_ERROR_DEF_H
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberStatus
#else
enum
#endif //DOXYGEN_SHOULD_SKIP_THIS
{
  EMBER_SUCCESS = 0x00,
  EMBER_ERR_FATAL = 0x01,
  EMBER_BAD_ARGUMENT = 0x02,
  EMBER_EEPROM_MFG_STACK_VERSION_MISMATCH = 0x04,
  EMBER_INVALID_CALL = 0x70,
  EMBER_EEPROM_MFG_VERSION_MISMATCH = 0x06,
  EMBER_EEPROM_STACK_VERSION_MISMATCH = 0x07,
  EMBER_NO_BUFFERS = 0x18,
  EMBER_SERIAL_INVALID_BAUD_RATE = 0x20,
  EMBER_SERIAL_INVALID_PORT = 0x21,
  EMBER_SERIAL_TX_OVERFLOW = 0x22,
  EMBER_SERIAL_RX_OVERFLOW = 0x23,
  EMBER_SERIAL_RX_FRAME_ERROR = 0x24,
  EMBER_SERIAL_RX_PARITY_ERROR = 0x25,
  EMBER_SERIAL_RX_EMPTY = 0x26,
  EMBER_SERIAL_RX_OVERRUN_ERROR = 0x27,
  EMBER_MAC_NO_DATA = 0x31,
  EMBER_MAC_SYNC_TIMEOUT = 0x33,
  EMBER_MAC_SYNC_WRONG_SEED = 0x34,
  EMBER_MAC_SECURITY_FAILED = 0x35,
  EMBER_MAC_UNKNOWN_DESTINATION = 0x37,
  EMBER_MAC_SECURITY_NOT_SUPPORTED = 0x38,
  EMBER_MAC_TRANSMIT_QUEUE_FULL = 0x39,
// Internal
  EMBER_MAC_ACK_HEADER_TYPE = 0x3B,
  EMBER_MAC_SCANNING = 0x3D,
  EMBER_MAC_BUSY = 0x3E,
  EMBER_MAC_NO_ACK_RECEIVED = 0x40,
  EMBER_MAC_INDIRECT_TIMEOUT = 0x41,
  EMBER_MAC_INDIRECT_MESSAGE_PURGED = 0x42,
  EMBER_SIM_EEPROM_ERASE_PAGE_GREEN = 0x43,
  EMBER_SIM_EEPROM_ERASE_PAGE_RED = 0x44,
  EMBER_SIM_EEPROM_FULL = 0x45,
//  Errors 46 and 47 are now defined below in the
//    flash error block (was attempting to prevent renumbering)
  EMBER_SIM_EEPROM_INIT_2_FAILED = 0x49,
  EMBER_SIM_EEPROM_INIT_3_FAILED = 0x4A,
  EMBER_SIM_EEPROM_REPAIRING = 0x4D,
  EMBER_ERR_FLASH_WRITE_INHIBITED = 0x46,
  EMBER_ERR_FLASH_VERIFY_FAILED = 0x47,
  EMBER_ERR_FLASH_PROG_FAIL = 0x4B,
  EMBER_MESSAGE_TOO_LONG = 0x74,
  EMBER_ADC_CONVERSION_DONE = 0x80,
  EMBER_ADC_CONVERSION_BUSY = 0x81,
  EMBER_ADC_CONVERSION_DEFERRED = 0x82,
  EMBER_ADC_NO_CONVERSION_PENDING = 0x84,
  EMBER_SLEEP_INTERRUPTED = 0x85,
  EMBER_PHY_TX_INCOMPLETE = 0x89,
  EMBER_PHY_INVALID_CHANNEL = 0x8A,
  EMBER_PHY_INVALID_POWER = 0x8B,
  EMBER_PHY_TX_BUSY = 0x8C,
  EMBER_PHY_TX_CCA_FAIL = 0x8D,
  EMBER_PHY_CALIBRATING = 0x8E,
  EMBER_PHY_ACK_RECEIVED = 0x8F,
  EMBER_NETWORK_UP = 0x90,
  EMBER_NETWORK_DOWN = 0x91,
  EMBER_JOIN_SCAN_FAILED = 0x92,
  EMBER_JOIN_FAILED = 0x94,
  EMBER_JOIN_DENIED = 0x95,
  EMBER_JOIN_TIMEOUT = 0x96,
  EMBER_NO_VALID_BEACONS = 0xAB,
  EMBER_SECURITY_DATA_INVALID = 0xBD,
  EMBER_NOT_JOINED = 0x93,
  EMBER_TABLE_FULL = 0xB4,
  EMBER_LIBRARY_NOT_PRESENT = 0xB5,
  EMBER_CHILD_NOT_FOUND = 0xB6,
  EMBER_NVM3_ERR_OPENED_WITH_OTHER_PARAMETERS = 0xC1,
  EMBER_NVM3_ERR_ALIGNMENT_INVALID = 0xC2,
  EMBER_NVM3_ERR_SIZE_TOO_SMALL = 0xC3,
  EMBER_NVM3_ERR_PAGE_SIZE_NOT_SUPPORTED = 0xC4,
  EMBER_NVM3_ERR_TOKEN_INIT = 0xC5,
  EMBER_NVM3_ERR_UPGRADE = 0xC6,
  EMBER_NVM3_ERR_UNKNOWN = 0xC7,
  EMBER_NCP_UNKNOWN_COMMAND_ID = 0xD0,
  EMBER_APPLICATION_ERROR_0 = 0xF0,
  EMBER_APPLICATION_ERROR_1 = 0xF1,
  EMBER_APPLICATION_ERROR_2 = 0xF2,
  EMBER_APPLICATION_ERROR_3 = 0xF3,
  EMBER_APPLICATION_ERROR_4 = 0xF4,
  EMBER_APPLICATION_ERROR_5 = 0xF5,
  EMBER_APPLICATION_ERROR_6 = 0xF6,
  EMBER_APPLICATION_ERROR_7 = 0xF7,
  EMBER_APPLICATION_ERROR_8 = 0xF8,
  EMBER_APPLICATION_ERROR_9 = 0xF9,
  EMBER_APPLICATION_ERROR_10 = 0xFA,
  EMBER_APPLICATION_ERROR_11 = 0xFB,
  EMBER_APPLICATION_ERROR_12 = 0xFC,
  EMBER_APPLICATION_ERROR_13 = 0xFD,
  EMBER_APPLICATION_ERROR_14 = 0xFE,
  EMBER_APPLICATION_ERROR_15 = 0xFF,
};
#endif // SILABS_ERROR_DEF_H
Enumerations#
Enumeration Documentation#
EmberStatus#
EmberStatus
| Enumerator | |
|---|---|
| EMBER_SUCCESS | The generic "no error" message. | 
| EMBER_ERR_FATAL | The generic "fatal error" message. | 
| EMBER_BAD_ARGUMENT | An invalid value was passed as an argument to a function. | 
| EMBER_EEPROM_MFG_STACK_VERSION_MISMATCH | The manufacturing and stack token format in non-volatile memory is different than what the stack expects (returned at initialization). | 
| EMBER_INVALID_CALL | The API call is not allowed given the current state of the stack. | 
| EMBER_EEPROM_MFG_VERSION_MISMATCH | The manufacturing token format in non-volatile memory is different than what the stack expects (returned at initialization). | 
| EMBER_EEPROM_STACK_VERSION_MISMATCH | The stack token format in non-volatile memory is different than what the stack expects (returned at initialization). | 
| EMBER_NO_BUFFERS | There are no more buffers (either in the stack heap or the queue used by the associated module, such as indirect queue). | 
| EMBER_SERIAL_INVALID_BAUD_RATE | Specified an invalid baud rate. | 
| EMBER_SERIAL_INVALID_PORT | Specified an invalid serial port. | 
| EMBER_SERIAL_TX_OVERFLOW | Tried to send too much data. | 
| EMBER_SERIAL_RX_OVERFLOW | There was not enough space to store a received character and some characters were dropped. | 
| EMBER_SERIAL_RX_FRAME_ERROR | Detected a UART framing error. | 
| EMBER_SERIAL_RX_PARITY_ERROR | Detected a UART parity error. | 
| EMBER_SERIAL_RX_EMPTY | There is no received data to process. | 
| EMBER_SERIAL_RX_OVERRUN_ERROR | The receive interrupt was not handled in time and some characters were dropped. | 
| EMBER_MAC_NO_DATA | No pending data exists for device doing a data poll. | 
| EMBER_MAC_SYNC_TIMEOUT | The frequency hopping client failed the frequency hopping synchronization procedure. It timed out trying to reach the frequency hopping server. | 
| EMBER_MAC_SYNC_WRONG_SEED | The frequency hopping client failed the frequency hopping synchronization procedure. The server is currently using a different seed. | 
| EMBER_MAC_SECURITY_FAILED | MAC security operation failed. | 
| EMBER_MAC_UNKNOWN_DESTINATION | Transmission failed: the destination node does not appear in the neighbor or child tables. | 
| EMBER_MAC_SECURITY_NOT_SUPPORTED | Transmission failed: the local node does not support security or a secured transmission has been requested to a child that does not support security. | 
| EMBER_MAC_TRANSMIT_QUEUE_FULL | The MAC transmit queue is full. | 
| EMBER_MAC_ACK_HEADER_TYPE | MAC ACK header received. | 
| EMBER_MAC_SCANNING | The MAC can't complete this task because it is scanning. | 
| EMBER_MAC_BUSY | The requested operation cannot be completed because MAC is currently busy performing a high-priority task. | 
| EMBER_MAC_NO_ACK_RECEIVED | Expected to receive an ACK following the transmission, but the MAC level ACK was never received. | 
| EMBER_MAC_INDIRECT_TIMEOUT | Indirect data message timed out before polled. | 
| EMBER_MAC_INDIRECT_MESSAGE_PURGED | Transmission failed: the indirect message was purged because the destination child has been removed or updated, or because emberPurgeIndirectMessages() was called. | 
| EMBER_SIM_EEPROM_ERASE_PAGE_GREEN | The Simulated EEPROM is telling the application that there is at least one flash page to be erased. The GREEN status means the current page has not filled above the ::ERASE_CRITICAL_THRESHOLD. | 
| EMBER_SIM_EEPROM_ERASE_PAGE_RED | The Simulated EEPROM is telling the application that there is at least one flash page to be erased. The RED status means the current page has filled above the ::ERASE_CRITICAL_THRESHOLD. | 
| EMBER_SIM_EEPROM_FULL | The Simulated EEPROM has run out of room to write any new data and the data trying to be set has been lost. This error code is the result of ignoring the EMBER_SIM_EEPROM_ERASE_PAGE_RED error code. | 
| EMBER_SIM_EEPROM_INIT_2_FAILED | Attempt 2 to initialize the Simulated EEPROM has failed. | 
| EMBER_SIM_EEPROM_INIT_3_FAILED | Attempt 3 to initialize the Simulated EEPROM has failed. | 
| EMBER_SIM_EEPROM_REPAIRING | The Simulated EEPROM is repairing itself. | 
| EMBER_ERR_FLASH_WRITE_INHIBITED | A fatal error has occurred while trying to write data to the flash. The target memory attempting to be programmed is already programmed. The flash write routines were asked to flip a bit from a 0 to 1, which is physically impossible and the write was therefore inhibited. The data in the flash cannot be trusted after this error. | 
| EMBER_ERR_FLASH_VERIFY_FAILED | A fatal error has occurred while trying to write data to the flash and the write verification has failed. The data in the flash cannot be trusted after this error, and it is possible this error is the result of exceeding the life cycles of the flash. | 
| EMBER_ERR_FLASH_PROG_FAIL | A fatal error has occurred while trying to write data to the flash, possibly due to write protection or an invalid address. The data in the flash cannot be trusted after this error, and it is possible this error is the result of exceeding the life cycles of the flash. | 
| EMBER_MESSAGE_TOO_LONG | The message to be transmitted is too big to fit into a single over-the-air packet. | 
| EMBER_ADC_CONVERSION_DONE | Conversion is complete. | 
| EMBER_ADC_CONVERSION_BUSY | Conversion cannot be done because a request is being processed. | 
| EMBER_ADC_CONVERSION_DEFERRED | Conversion is deferred until the current request has been processed. | 
| EMBER_ADC_NO_CONVERSION_PENDING | No results are pending. | 
| EMBER_SLEEP_INTERRUPTED | Sleeping (for a duration) has been abnormally interrupted and exited prematurely. | 
| EMBER_PHY_TX_INCOMPLETE | The transmit hardware did not finish transmitting a packet. | 
| EMBER_PHY_INVALID_CHANNEL | An unsupported channel setting was specified. | 
| EMBER_PHY_INVALID_POWER | An unsupported power setting was specified. | 
| EMBER_PHY_TX_BUSY | The requested operation cannot be completed because the radio is currently busy, either transmitting a packet or performing calibration. | 
| EMBER_PHY_TX_CCA_FAIL | The transmit attempt failed because all CCA attempts indicated that the channel was busy. | 
| EMBER_PHY_CALIBRATING | The requested operation cannot be completed because the stack has triggered a radio calibration. Wait for about one second for it to complete. | 
| EMBER_PHY_ACK_RECEIVED | The expected ACK was received after the last transmission. | 
| EMBER_NETWORK_UP | The stack software has completed initialization required to be in a network and is ready to send and receive packets over the air. | 
| EMBER_NETWORK_DOWN | The network is not operating. | 
| EMBER_JOIN_SCAN_FAILED | The node failed to initiate the scanning process during the joining process. | 
| EMBER_JOIN_FAILED | An attempt to join a network failed. | 
| EMBER_JOIN_DENIED | An attempt to join a network was rejected. | 
| EMBER_JOIN_TIMEOUT | The node timed out waiting for a response during the joining process. | 
| EMBER_NO_VALID_BEACONS | An attempt to join or rejoin the network failed because no valid beacons was received by the joining node. | 
| EMBER_SECURITY_DATA_INVALID | The security data provided was not valid, or an integrity check failed. | 
| EMBER_NOT_JOINED | The node has not joined a network. Returned by emberNetworkInit() if there was no connection data saved in tokens. | 
| EMBER_TABLE_FULL | There are no empty entries left in the table. | 
| EMBER_LIBRARY_NOT_PRESENT | The requested function cannot be executed because the library (plugin) that contains the necessary functionality is not present. | 
| EMBER_CHILD_NOT_FOUND | The requested NodeId has not been found in the child list or grandchildren list (start network only). | 
| EMBER_NVM3_ERR_OPENED_WITH_OTHER_PARAMETERS | NVM3 is telling the application that the initialization was aborted as the NVM3 instance was already opened with other parameters. | 
| EMBER_NVM3_ERR_ALIGNMENT_INVALID | NVM3 is telling the application that the initialization was aborted as the NVM3 instance is not aligned properly in memory. | 
| EMBER_NVM3_ERR_SIZE_TOO_SMALL | NVM3 is telling the application that the initialization was aborted as the size of the NVM3 instance is too small. | 
| EMBER_NVM3_ERR_PAGE_SIZE_NOT_SUPPORTED | NVM3 is telling the application that the initialization was aborted as the NVM3 page size is not supported. | 
| EMBER_NVM3_ERR_TOKEN_INIT | NVM3 is telling the application that there was an error initializing some of the tokens. | 
| EMBER_NVM3_ERR_UPGRADE | NVM3 is telling the application there has been an error when attempting to upgrade SimEE tokens. | 
| EMBER_NVM3_ERR_UNKNOWN | NVM3 is telling the application that there has been an unknown error. | 
| EMBER_NCP_UNKNOWN_COMMAND_ID | The NCP does not know the command ID that the host sent. This can correspond to a version mismatch, where an API is available on the host but not on the NCP. | 
| EMBER_APPLICATION_ERROR_0 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_1 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_2 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_3 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_4 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_5 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_6 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_7 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_8 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_9 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_10 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_11 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_12 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_13 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_14 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. | 
| EMBER_APPLICATION_ERROR_15 | This error is reserved for customer application use. This will never be returned from any portion of the network stack or HAL. |