/***************************************************************************/
#ifndef RADIO_STREAM_H
#define RADIO_STREAM_H
EmberStatus emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel);
EmberStatus emberStopTxStream(void);
#endif
Functions#
emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel)
Start a continuous TX stream to test RF.
emberStopTxStream(void)
Stop an RF stream in progress.
Function Documentation#
emberStartTxStream#
EmberStatus emberStartTxStream (EmberTxStreamParameters parameters, uint16_t channel)
Start a continuous TX stream to test RF.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberTxStreamParameters | [in] | parameters | Stream mode. See EmberTxStreamParameters. |
| uint16_t | [in] | channel | RF channel. |
Returns
EMBER_INVALID_CALL if the stack can not process the request EMBER_BAD_ARGUMENT if the parameters are wrong EMBER_SUCCESS if the stream can be started
emberStopTxStream#
EmberStatus emberStopTxStream (void )
Stop an RF stream in progress.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
EMBER_INVALID_CALL if no stream is in progress EMBER_SUCCESS otherwise