Full HAL functions common across all microcontroller-specific files. See Common Microcontroller Functions for documentation.
Some functions in this file return an EmberStatus value. See error-def.h for definitions of all EmberStatus return values.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef __MICRO_H__
#define __MICRO_H__
#include "hal/micro/generic/em2xx-reset-defs.h"
#include "hal/micro/micro-types.h"
#ifndef DOXYGEN_SHOULD_SKIP_THIS
// Make sure that a proper plat/micro combination was selected if we aren't
// building for a host processor
#if ((!defined(EZSP_HOST)) && (!defined(UNIX_HOST)))
#ifndef PLAT
#error no platform defined, or unsupported
#endif
#ifndef MICRO
#error no micro defined, or unsupported
#endif
#ifndef PHY
#error no phy defined, or unsupported
#endif
#endif // ((! defined(EZSP_HOST)) && (! defined(UNIX_HOST)))
#endif // DOXYGEN_SHOULD_SKIP_THIS
void halStackProcessBootCount(void);
uint8_t halGetResetInfo(void);
PGM_P halGetResetString(void);
#if defined(CORTEXM3)
uint8_t halGetEm2xxResetInfo(void);
#else
#define halGetEm2xxResetInfo() halGetResetInfo()
#endif
#ifndef DOXYGEN_SHOULD_SKIP_THIS
#include "micro-common.h"
#if defined(EMBER_TEST)
#include "hal/micro/unix/simulation/micro.h"
#include "hal/micro/unix/simulation/bootloader.h"
#elif defined(CORTEXM3_EFM32_MICRO)
#include "cortexm3/efm32/micro.h"
#elif ((defined(EZSP_HOST) || defined(UNIX_HOST)))
#include "hal/micro/unix/host/micro.h"
#else
#error no platform or micro defined
#endif
// the number of ticks (as returned from halCommonGetInt32uMillisecondTick)
// that represent an actual second. This can vary on different platforms.
// It must be defined by the host system.
#ifndef MILLISECOND_TICKS_PER_SECOND
#define MILLISECOND_TICKS_PER_SECOND 1024UL
// See bug 10232
// #error "MILLISECOND_TICKS_PER_SECOND is not defined in micro.h!"
#endif
#ifndef MILLISECOND_TICKS_PER_DECISECOND
#define MILLISECOND_TICKS_PER_DECISECOND (MILLISECOND_TICKS_PER_SECOND / 10)
#endif
#ifndef MILLISECOND_TICKS_PER_QUARTERSECOND
#define MILLISECOND_TICKS_PER_QUARTERSECOND (MILLISECOND_TICKS_PER_SECOND >> 2)
#endif
#ifndef MILLISECOND_TICKS_PER_MINUTE
#define MILLISECOND_TICKS_PER_MINUTE (60UL * MILLISECOND_TICKS_PER_SECOND)
#endif
#ifndef MILLISECOND_TICKS_PER_HOUR
#define MILLISECOND_TICKS_PER_HOUR (60UL * MILLISECOND_TICKS_PER_MINUTE)
#endif
#ifndef MILLISECOND_TICKS_PER_DAY
#define MILLISECOND_TICKS_PER_DAY (24UL * MILLISECOND_TICKS_PER_HOUR)
#endif
#endif // DOXYGEN_SHOULD_SKIP_THIS
#endif //__MICRO_H__
Macros#
Calls ::halGetExtendedResetInfo() and translates the EM35x reset code to the corresponding value used by the EM2XX HAL. Any reset codes not present in the EM2XX are returned after being OR'ed with 0x80.
Functions#
Called from emberInit and provides a means for the HAL to increment a boot counter, most commonly in non-volatile memory.
Gets information about what caused the microcontroller to reset.
Calls halGetResetInfo() and supplies a string describing it.
Macro Definition Documentation#
halGetEm2xxResetInfo#
#define halGetEm2xxResetInfoValue:
()
Calls ::halGetExtendedResetInfo() and translates the EM35x reset code to the corresponding value used by the EM2XX HAL. Any reset codes not present in the EM2XX are returned after being OR'ed with 0x80.
Application Usage:\n Used by the EZSP host as a platform-independent NCP reset code.#
Returns
The EM2XX-compatible reset code. If not supported by the EM2XX, return the platform-specific code with B7 set.
Function Documentation#
halStackProcessBootCount#
void halStackProcessBootCount (void )
Called from emberInit and provides a means for the HAL to increment a boot counter, most commonly in non-volatile memory.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This is useful while debugging to determine the number of resets that might be seen over a period of time. Exposing this functionality allows the application to disable or alter processing of the boot counter if, for example, the application is expecting a lot of resets that could wear out non-volatile storage or some
EmberStack Usage:\n Called from emberInit only as helpful debugging information.#
This should be left enabled by default, but this function can also be reduced to a simple return statement if boot counting is not desired.
halGetResetInfo#
uint8_t halGetResetInfo (void )
Gets information about what caused the microcontroller to reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A code identifying the cause of the reset.
halGetResetString#
PGM_P halGetResetString (void )
Calls halGetResetInfo() and supplies a string describing it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Application Usage:\n Useful for diagnostic printing of text just after program#
initialization.
Returns
A pointer to a program space string.