/***************************************************************************/
#ifndef RADIO_STREAM_H
#define RADIO_STREAM_H

EmberStatus emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel);

EmberStatus emberStopTxStream(void);

 #endif

Functions#

emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel)

Start a continuous TX stream to test RF.

Stop an RF stream in progress.

Function Documentation#

emberStartTxStream#

EmberStatus emberStartTxStream (EmberTxStreamParameters parameters, uint16_t channel)

Start a continuous TX stream to test RF.

Parameters
[in]parameters

Stream mode. See EmberTxStreamParameters.

[in]channel

RF channel.

Returns

  • EMBER_INVALID_CALL if the stack can not process the request EMBER_BAD_ARGUMENT if the parameters are wrong EMBER_SUCCESS if the stream can be started


Definition at line 50 of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/radio-stream.h

emberStopTxStream#

EmberStatus emberStopTxStream (void )

Stop an RF stream in progress.

Parameters
N/A

Returns

  • EMBER_INVALID_CALL if no stream is in progress EMBER_SUCCESS otherwise


Definition at line 58 of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/radio-stream.h