/***************************************************************************/
#ifndef __ERRORS_H__
#define __ERRORS_H__

#include "include/error-def.h"

#ifndef __EMBERSTATUS_TYPE__
#define __EMBERSTATUS_TYPE__
typedef uint8_t EmberStatus;
#endif //__EMBERSTATUS_TYPE__

#endif // __ERRORS_H__

Macros#

#define

Return codes for Ember Connect API functions and module definitions.

Typedefs#

typedef uint8_t

Macro Definition Documentation#

__EMBERSTATUS_TYPE__#

#define __EMBERSTATUS_TYPE__

Return codes for Ember Connect API functions and module definitions.

See Status Codes for documentation.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.

  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.

  3. This notice may not be removed or altered from any source distribution.

Return type for Ember functions.


Definition at line 41 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/error.h

Typedef Documentation#

EmberStatus#

typedef uint8_t EmberStatus

Definition at line 42 of file /mnt/raid/workspaces/ws.hNs8xjOxH/overlay/gsdk/protocol/flex/stack/include/error.h